Transport layer initialization.
More...
Transport layer initialization.
|
|
typedef struct ErpcTransport * | erpc_transport_t |
| | Opaque transport object type.
|
| |
|
typedef void(* | rpmsg_ready_cb) (void) |
| | Ready callback object type for RPMsg-Lite transport.
|
| |
|
| erpc_transport_t | erpc_transport_rpmsg_lite_master_init (uint32_t src_addr, uint32_t dst_addr, uint32_t rpmsg_link_id) |
| | Create an RPMsg-Lite transport. More...
|
| |
| erpc_transport_t | erpc_transport_rpmsg_lite_remote_init (uint32_t src_addr, uint32_t dst_addr, void *start_address, uint32_t rpmsg_link_id, rpmsg_ready_cb ready, char *nameservice_name) |
| | Create an RPMsg-Lite transport. More...
|
| |
| erpc_transport_t | erpc_transport_rpmsg_lite_rtos_master_init (uint32_t src_addr, uint32_t dst_addr, uint32_t rpmsg_link_id) |
| | Create an RPMsg-Lite RTOS transport. More...
|
| |
| erpc_transport_t | erpc_transport_rpmsg_lite_rtos_remote_init (uint32_t src_addr, uint32_t dst_addr, void *start_address, uint32_t rpmsg_link_id, rpmsg_ready_cb ready, char *nameservice_name) |
| | Create an RPMsg-Lite RTOS transport. More...
|
| |
| erpc_transport_t | erpc_transport_rpmsg_lite_tty_rtos_remote_init (uint32_t src_addr, uint32_t dst_addr, void *start_address, uint32_t rpmsg_link_id, rpmsg_ready_cb ready, char *nameservice_name) |
| | Create an RPMsg-Lite TTY transport. More...
|
| |
| void | erpc_transport_rpmsg_lite_tty_rtos_deinit (void) |
| | Deinitialize an RPMSG lite tty rtos transport. More...
|
| |
Create a CMSIS UART transport.
Create a CMSIS UART transport instance, to be used on both the server and the client side.
- Parameters
-
| [in] | uartDrv | CMSIS USART driver structure address (Driver Control Block). |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_serial_init |
( |
const char * |
portName, |
|
|
long |
baudRate |
|
) |
| |
Create a host PC serial port transport.
Create a host PC serial port transport instance.
- Parameters
-
| [in] | portName | Port name. |
| [in] | baudRate | Baud rate. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_spi_master_init |
( |
void * |
baseAddr, |
|
|
uint32_t |
baudRate, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
Create a SPI master transport.
Create SPI master transport instance, to be used at master core.
- Parameters
-
| [in] | baseAddr | Base address of SPI peripheral used in this transport layer. |
| [in] | baudRate | SPI baud rate. |
| [in] | srcClock_Hz | SPI source clock in Hz. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_spi_slave_init |
( |
void * |
baseAddr, |
|
|
uint32_t |
baudRate, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
Create a SPI slave transport.
Create SPI slave transport instance, to be used at slave core.
- Parameters
-
| [in] | baseAddr | Base address of SPI peripheral used in this transport layer. |
| [in] | baudRate | SPI baud rate. |
| [in] | srcClock_Hz | SPI source clock in Hz. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_dspi_master_init |
( |
void * |
baseAddr, |
|
|
uint32_t |
baudRate, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
Create a DSPI master transport.
Create DSPI master transport instance, to be used at master core.
- Parameters
-
| [in] | baseAddr | Base address of DSPI peripheral used in this transport layer. |
| [in] | baudRate | DSPI baud rate. |
| [in] | srcClock_Hz | DSPI source clock in Hz. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_dspi_slave_init |
( |
void * |
baseAddr, |
|
|
uint32_t |
baudRate, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
Create a DSPI slave transport.
Create DSPI slave transport instance, to be used at slave core.
- Parameters
-
| [in] | baseAddr | Base address of DSPI peripheral used in this transport layer. |
| [in] | baudRate | DSPI baud rate. |
| [in] | srcClock_Hz | DSPI source clock in Hz. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
Create an MU transport.
Create Messaging Unit (MU) transport instance, to be used on both the server and the client side. Base address of the MU peripheral needs to be passed.
- Parameters
-
| [in] | baseAddr | Base address of MU peripheral. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_rpmsg_lite_master_init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
uint32_t |
rpmsg_link_id |
|
) |
| |
Create an RPMsg-Lite transport.
Create RPMsg-Lite baremetal transport instance, to be used at master core.
- Parameters
-
| [in] | src_addr | Address of local RPMsg endpoint used for communication. |
| [in] | dst_addr | Address of remote RPMsg endpoint used for communication. |
| [in] | rpmsg_link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_rpmsg_lite_remote_init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
void * |
start_address, |
|
|
uint32_t |
rpmsg_link_id, |
|
|
rpmsg_ready_cb |
ready, |
|
|
char * |
nameservice_name |
|
) |
| |
Create an RPMsg-Lite transport.
Create RPMsg-Lite baremetal transport instance, to be used at slave/remote core.
- Parameters
-
| [in] | src_addr | Address of local RPMsg endpoint used for communication. |
| [in] | dst_addr | Address of remote RPMsg endpoint used for communication. |
| [in] | start_address | Shared memory base address used for this instance of RPMsg-Lite. |
| [in] | rpmsg_link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h. |
| [in] | ready | Callback function, which gets called, when RPMsg is initialized and master core can be notified. |
| [in] | nameservice_name | Name of the nameservice channel to be announced to the other core. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_rpmsg_lite_rtos_master_init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
uint32_t |
rpmsg_link_id |
|
) |
| |
Create an RPMsg-Lite RTOS transport.
Create RPMsg-Lite RTOS transport instance, to be used at master core.
- Parameters
-
| [in] | src_addr | Address of local RPMsg endpoint used for communication. |
| [in] | dst_addr | Address of remote RPMsg endpoint used for communication. |
| [in] | rpmsg_link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_rpmsg_lite_rtos_remote_init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
void * |
start_address, |
|
|
uint32_t |
rpmsg_link_id, |
|
|
rpmsg_ready_cb |
ready, |
|
|
char * |
nameservice_name |
|
) |
| |
Create an RPMsg-Lite RTOS transport.
Create RPMsg-Lite RTOS transport instance, to be used at slave/remote core.
- Parameters
-
| [in] | src_addr | Address of local RPMsg endpoint used for communication. |
| [in] | dst_addr | Address of remote RPMsg endpoint used for communication. |
| [in] | start_address | Shared memory base address used for this instance of RPMsg-Lite. |
| [in] | rpmsg_link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h. |
| [in] | ready | Callback function, which gets called, when RPMsg is initialized and master core can be notified. |
| [in] | nameservice_name | Name of the nameservice channel to be announced to the other core. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| erpc_transport_t erpc_transport_rpmsg_lite_tty_rtos_remote_init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
void * |
start_address, |
|
|
uint32_t |
rpmsg_link_id, |
|
|
rpmsg_ready_cb |
ready, |
|
|
char * |
nameservice_name |
|
) |
| |
Create an RPMsg-Lite TTY transport.
Create RPMsg-Lite TTY transport instance, to be used at slave/remote core. This function is mainly used with Linux running on the master core.
- Parameters
-
| [in] | src_addr | Address of local RPMsg endpoint used for communication. |
| [in] | dst_addr | Address of remote RPMsg endpoint used for communication. |
| [in] | start_address | Shared memory base address used for this instance of RPMsg-Lite. |
| [in] | rpmsg_link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h. |
| [in] | ready | Callback function, which gets called, when RPMsg is initialized and master core can be notified. |
| [in] | nameservice_name | Name of the nameservice channel to be announced to the other core. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| void erpc_transport_rpmsg_lite_tty_rtos_deinit |
( |
void |
| ) |
|
Deinitialize an RPMSG lite tty rtos transport.
This function deinitializes the RPMSG lite tty rtos transport.
| erpc_transport_t erpc_transport_rpmsg_linux_init |
( |
int16_t |
local_addr, |
|
|
int8_t |
type, |
|
|
int16_t |
remote_addr |
|
) |
| |
Create an Linux RPMSG endpoint transport.
This function is using RPMSG endpoints based on this implementation: https://github.com/NXPmicro/rpmsg-sysfs/tree/0aa1817545a765c200b1b2f9b6680a420dcf9171 .
When local/remote address is set to '-1', then default addresses will be used. When type is set to '0', then Datagram model will be used, else Stream.
- Parameters
-
| [in] | local_addr | Local endpoint address. |
| [in] | type | Datagram (0) or Stream (1). |
| [in] | remote_addr | Remote endpoint address. |
- Returns
- Return NULL or erpc_transport_t instance pointer.
| void erpc_transport_rpmsg_linux_deinit |
( |
void |
| ) |
|
Deinitialize an Linux RPMSG endpoint transport.
This function deinitializes the Linux RPMSG endpoint transport.