![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
64-bit integer value. More...
#include <Value.h>
Public Types | |
| enum | int_type_t { kSigned, kSignedLong, kUnsigned, kUnsignedLong } |
| Supported sizes of integers. | |
Public Member Functions | |
| IntegerValue (int_type_t type=kSigned) | |
| Constructor. | |
| IntegerValue (uint64_t value, int_type_t type=kSigned) | |
| Constructor. More... | |
| IntegerValue (const IntegerValue &other) | |
| Copy constructor. More... | |
| virtual std::string | getTypeName () const |
| Get IntegerValue type name. More... | |
| virtual size_t | getSize () const |
| Get IntegerValue type size. More... | |
| uint64_t | getValue () const |
| This function returns value. More... | |
| int_type_t | getIntType () |
| This function returns signed/unsigned type. More... | |
| operator uint64_t () const | |
| Casting operator. More... | |
| IntegerValue & | operator= (int64_t value) |
| Assign operator. More... | |
| virtual std::string | toString () const |
| Get IntegerValue type string representation. More... | |
| virtual Value * | clone () const |
| Clone IntegerValue. More... | |
Public Member Functions inherited from Value | |
| Value (value_type_t theType) | |
| Constructor. More... | |
| virtual | ~Value () |
| Destructor. | |
| virtual value_type_t | getType () const |
| Get Value type. More... | |
Protected Attributes | |
| uint64_t | m_value |
| The integer value. | |
| int_type_t | m_intType |
| The integer type. | |
64-bit integer value.
|
inline |
Constructor.
| [in] | value | IntegerValue value. |
|
inline |
Copy constructor.
| [in] | other | IntegerValue to copy. |
|
inlinevirtual |
|
inline |
This function returns signed/unsigned type.
|
inlinevirtual |
|
inlinevirtual |
|
inline |
This function returns value.
|
inline |
Casting operator.
|
inline |
|
inlinevirtual |
Get IntegerValue type string representation.
Implements Value.