![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
Wraps a set of static functions for easy global logging access. More...
#include <Logging.h>
Classes | |
| class | SetOutputLevel |
| Utility class to temporarily change the logging output level. More... | |
Static Public Member Functions | |
Singleton logger access | |
| static Logger * | getLogger () |
| Returns the current global logger singleton. | |
| static void | setLogger (Logger *logger) |
| Sets the global logger singleton instance. | |
Logging | |
| static void | log (const char *fmt,...) |
| Log with format. | |
| static void | log (const std::string &msg) |
| Log a string object. | |
| static void | log (Logger::log_level_t level, const char *fmt,...) |
| Log with format at a specific output level. | |
| static void | log (Logger::log_level_t level, const std::string &msg) |
| Log a string output at a specific output level. | |
Logging level helpers | |
These static methods log a message with an implicit log level. | |
| static void | urgent (const char *fmt,...) |
| Log a message with Logger::kUrgent level. | |
| static void | error (const char *fmt,...) |
| Log a message with Logger::kError level. | |
| static void | warning (const char *fmt,...) |
| Log a message with Logger::kWarning level. | |
| static void | info (const char *fmt,...) |
| Log a message with Logger::kInfo level. | |
| static void | info2 (const char *fmt,...) |
| Log a message with Logger::kInfo2 level. | |
| static void | debug (const char *fmt,...) |
| Log a message with Logger::kDebug level. | |
| static void | debug2 (const char *fmt,...) |
| Log a message with Logger::kDebug2 level. | |
Static Protected Attributes | |
| static Logger * | s_logger |
| The single global logger instance. | |
Wraps a set of static functions for easy global logging access.
This class has a set of static methods that make it easy to access a global logger instance without having to worry about extern symbols. It does this by keeping a static member variable pointing at the singleton logger instance, which is set with the setLogger() static method.
There is also an inner utility class called SetOutputLevel that uses C++ scoping rules to temporarily change the output logging level. When the SetOutputLevel instance falls out of scope the output level is restored to the previous value.