![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
#include <options.h>
Public Member Functions | |
| virtual const char * | curr (void)=0 |
| virtual void | next (void)=0 |
| next() advances to the next item. | |
| virtual const char * | operator() (void)=0 |
| virtual void | rewind (void)=0 |
| rewind() resets the "current-element" to the first one in the "list" | |
Abstract class for a rewindable OptIter
|
pure virtual |
curr() returns the current item in the iterator without advancing on to the next item. If we are at the end of items then NULL is returned.
Implements OptIter.
Implemented in OptStrTokIter, and OptArgvIter.
|
pure virtual |
operator() returns the current item in the iterator and then advances on to the next item. If we are at the end of items then NULL is returned.
Reimplemented from OptIter.
Implemented in OptStrTokIter, and OptArgvIter.