![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
Handles searching a list of paths for a file. More...
#include <SearchPath.h>
Public Types | |
| enum | _target_type { kFindFile, kFindDirectory } |
| typedef enum _target_type | target_type_t |
Public Member Functions | |
| PathSearcher () | |
| Constructor. | |
| void | addSearchPath (const std::string &path) |
| Add a new search path to the end of the list. | |
| void | setTempPath (const std::string &path) |
| Set temporary path. | |
| bool | search (const std::string &base, target_type_t targetType, bool searchCwd, std::string &result) |
| Attempts to locate a file by using the search paths. More... | |
Static Public Member Functions | |
| static PathSearcher & | getGlobalSearcher () |
| Access global path searching object. More... | |
Protected Types | |
| typedef std::list< std::string > | string_list_t |
| Linked list of strings. | |
Protected Member Functions | |
| bool | isAbsolute (const std::string &path) |
| Returns whether path is absolute. | |
| std::string | joinPaths (const std::string &first, const std::string &second) |
| Combines two paths into a single one. | |
Protected Attributes | |
| string_list_t | m_paths |
| Ordered list of paths to search. | |
| std::string | m_tempPath |
| Possibility to add temporary path. | |
Static Protected Attributes | |
| static PathSearcher * | s_searcher |
| Global search object singleton. | |
Handles searching a list of paths for a file.
| typedef enum _target_type PathSearcher::target_type_t |
Type of searched item.
|
static |
Access global path searching object.
This function will create the global path search object if it has not already been created.
| bool PathSearcher::search | ( | const std::string & | base, |
| target_type_t | targetType, | ||
| bool | searchCwd, | ||
| std::string & | result | ||
| ) |
Attempts to locate a file by using the search paths.
The base path argument can be either a relative or absolute path. If the path is relative, then it is joined with search paths one after another until a matching file is located or all search paths are exhausted. If the base is absolute, only that path is tested and if invalid false is returned.
| base | A path to the file that is to be found. | |
| targetType | Currently ignored. In the future it will let you select whether to find a file or directory. | |
| searchCwd | If set to true, the current working directory is searched before using any of the search paths. Otherwise only the search paths are considered. | |
| [out] | result | When true is returned this string is set to the first path at which a valid file was found. |
| true | A matching file was found among the search paths. The contents of result are a valid path. |
| false | No match could be made. result has been left unmodified. |