![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
Const class. More...
#include <ConstType.h>
Public Member Functions | |
| ConstType (const Token &tok, DataType *dataType, Value *value) | |
| Constructor. More... | |
| DataType * | getDataType () |
| This function returns pointer to element data type. More... | |
| Value * | getValue () |
| This function returns value of constant data type. More... | |
| void | setDataType (DataType *dataType) |
| This function sets constant data type. More... | |
| void | setValue (Value *value) |
| This function sets constant value. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| virtual bool | isBuiltin () const |
| This function return "false" value as default for identify builtin type. More... | |
| virtual std::string | getDescription () const |
| This function returns description about the symbol (symbol name). More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (std::string name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (std::string name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (std::string comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (std::string comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Protected Attributes | |
| DataType * | m_dataType |
| Value * | m_value |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Additional Inherited Members | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol, kAliasTypeSymbol, kArrayTypeSymbol, kBuiltinTypeSymbol, kEnumTypeSymbol, kFunctionTypeSymbol, kListTypeSymbol, kStructTypeSymbol, kUnionTypeSymbol } |
| Supported symbol types. | |
Const class.
Constructor.
This function set symbol token to given token, data type to given data type and value to given value.
| [in] | tok | Token, which contains name and location. |
| [in] | dataType | Given data type.. |
| [in] | value | Given value. |
|
inline |
This function returns pointer to element data type.
|
inline |
This function returns value of constant data type.
|
inline |
This function sets constant data type.
| [in] | dataType | Constant data type. |
|
inline |
This function sets constant value.
| [in] | value | Constant value. |
|
protected |
Constant data type.
|
protected |
Constant value.