![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
This class contains necessary information about analyzed file. More...
#include <ErpcLexer.h>
Public Member Functions | |
| CurrentFileInfo (std::ifstream *savedFile, std::string fileName, std::string currentFolderPath) | |
| Constructor. More... | |
| ~CurrentFileInfo () | |
| Destructor. More... | |
Public Attributes | |
| smart_ptr< std::ifstream > | m_savedFile |
| CurrentFileInfo * | m_previous |
| int | m_line |
| int | m_column |
| std::string | m_fileName |
| std::string | m_currentFolderPath |
This class contains necessary information about analyzed file.
|
inline |
Constructor.
This function set default values to object variables. Pointer to file ifstream, file name and current folder path are given as function parameters.
| [in] | savedFile | Pointer to analyzed file. |
| [in] | fileName | Name of analyzed file. |
| [in] | currentFolderPath | Path to folder of current file. |
|
inline |
Destructor.
This function will close used file, when destructor is called.
| int erpcgen::CurrentFileInfo::m_column |
Column number on the line in current file.
| std::string erpcgen::CurrentFileInfo::m_currentFolderPath |
Path to folder of current file.
| std::string erpcgen::CurrentFileInfo::m_fileName |
File name for current file.
| int erpcgen::CurrentFileInfo::m_line |
Line number in current file.
| CurrentFileInfo* erpcgen::CurrentFileInfo::m_previous |
Pointer to previous saved file info.
| smart_ptr<std::ifstream> erpcgen::CurrentFileInfo::m_savedFile |
Pointer to current file