![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
#include <Function.h>
Public Member Functions | |
| Function (const Token &tok, Interface *interface) | |
| Constructor. More... | |
| Function (const Token &tok, Interface *interface, uint32_t uniqueId) | |
| Constructor. More... | |
| uint32_t | getUniqueId () const |
| This function returns function unique id. More... | |
| void | setUniqueId (uint32_t newId) |
| This function set function unique id. More... | |
| Interface * | getInterface () const |
| This function returns parent Interface. More... | |
| virtual std::string | getDescription () const |
| This function returns description about the interface function. More... | |
| void | setFunctionType (FunctionType *functionType) |
| This function sets FunctionType (callback type). More... | |
| FunctionType * | getFunctionType () const |
| This function returns FunctionType (callback type). More... | |
Public Member Functions inherited from erpcgen::FunctionBase | |
| FunctionBase () | |
| Constructor. | |
| StructType & | getParameters () |
| This function returns function parameters. More... | |
| DataType * | getReturnType () |
| This function returns data type of function return value. More... | |
| StructMember * | getReturnStructMemberType () |
| This function returns data type of function return value. More... | |
| void | setReturnStructMemberType (StructMember *returnType) |
| This function set data type of function return value. More... | |
| bool | isOneway () const |
| This function returns true/false, when function return type is/isn't oneway. More... | |
| void | setIsOneway (bool isOneway) |
| This function set true/false, when function return type is/isn't oneway. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| virtual bool | isBuiltin () const |
| This function return "false" value as default for identify builtin type. More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (std::string name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (std::string name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (std::string comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (std::string comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Protected Attributes | |
| uint32_t | m_uniqueId |
| Interface * | m_interface |
| FunctionType * | m_functionType |
Protected Attributes inherited from erpcgen::FunctionBase | |
| StructType | m_parameters |
| StructMember * | m_returnType |
| bool | m_isOneway |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Static Protected Attributes | |
| static uint32_t | s_idCounter |
Additional Inherited Members | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol, kAliasTypeSymbol, kArrayTypeSymbol, kBuiltinTypeSymbol, kEnumTypeSymbol, kFunctionTypeSymbol, kListTypeSymbol, kStructTypeSymbol, kUnionTypeSymbol } |
| Supported symbol types. | |
Function declaration.
The function's parameters are represented by a StructType object.
Constructor.
This function set symbol token to given token.
| [in] | tok | Given token. |
| [in] | m_interface | Parent interface. |
Constructor.
This function set symbol token to given token, uniqueId and idCounter to given uniqueId.
| [in] | tok | Given token. |
| [in] | m_interface | Parent interface. |
| [in] | uniqueId | Given unique function id. |
|
virtual |
This function returns description about the interface function.
Implements erpcgen::FunctionBase.
|
inline |
This function returns FunctionType (callback type).
|
inline |
|
inline |
This function returns function unique id.
|
inline |
This function sets FunctionType (callback type).
| [in] | functionType | FunctionType (callback type). |
|
inline |
This function set function unique id.
| [in] | newId | New function unique id. |
|
protected |
Parent interface.
|
protected |
Parent interface.
|
protected |
Function unique id.
|
staticprotected |
Function id counter. Each function will increase this.