![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
An interface that contains functions. More...
#include <Group.h>
Public Types | |
| typedef std::vector< Interface * > | interface_list_t |
| typedef std::vector< Symbol * > | symbols_list_t |
| typedef std::map< Symbol *, std::set< _param_direction > > | symbol_directions_map_t |
Public Member Functions | |
| Group (const std::string name) | |
| Constructor. More... | |
| const std::string & | getName () const |
| This function returns the group name. More... | |
| void | addInterface (Interface *iface) |
| This function will add pointer to interface into vector of group interfaces. More... | |
| const interface_list_t & | getInterfaces () const |
| This function returns vector with pointers to interfaces belonging to the group. More... | |
| void | addDirToSymbolsMap (Symbol *symbol, _param_direction dir) |
| This function will add direction for specified symbol held in a symbol map. More... | |
| const std::set< _param_direction > | getSymbolDirections (Symbol *symbol) const |
| This function returns set with symbol directions. More... | |
| const symbols_list_t & | getSymbols () const |
| This function returns vector with symbols. More... | |
| void | setTemplate (cpptempl::data_map groupTemplate) |
| This function will set group template. More... | |
| cpptempl::data_map & | getTemplate () |
| This function returns group template. More... | |
| std::string | getDescription () const |
| This function returns description about the interface. More... | |
An interface that contains functions.
| typedef std::vector<Interface *> erpcgen::Group::interface_list_t |
Vector of interfaces belongs to group.
| typedef std::map<Symbol *, std::set<_param_direction> > erpcgen::Group::symbol_directions_map_t |
Map symbol with direction in which is used in current group.
| typedef std::vector<Symbol *> erpcgen::Group::symbols_list_t |
Vector of symbols belongs to group.
|
inline |
Constructor.
| [in] | name | Group name. |
| void Group::addDirToSymbolsMap | ( | Symbol * | symbol, |
| _param_direction | dir | ||
| ) |
This function will add direction for specified symbol held in a symbol map.
| [in] | symbol | Symbol for which direction should be added. |
| [in] | dir | Direction of the symbol. |
| void Group::addInterface | ( | Interface * | iface | ) |
This function will add pointer to interface into vector of group interfaces.
| [in] | iface | Pointer to interface. |
| string Group::getDescription | ( | ) | const |
This function returns description about the interface.
|
inline |
This function returns vector with pointers to interfaces belonging to the group.
|
inline |
This function returns the group name.
| const set< _param_direction > Group::getSymbolDirections | ( | Symbol * | symbol | ) | const |
This function returns set with symbol directions.
| [in] | symbol | Symbol which direction set should be returned. |
|
inline |
This function returns vector with symbols.
Unique symbols are added into vector within addDirToSymbolsMap() function.
|
inline |
This function returns group template.
| void Group::setTemplate | ( | cpptempl::data_map | groupTemplate | ) |
This function will set group template.
| [in] | groupTemplate | Group template defined as data map. |