![]() |
eRPC Generator (erpcgen)
Rev. 1.7.4
NXP Semiconductors
|
Discriminated union case type. More...
#include <UnionCase.h>
Public Member Functions | |
| UnionCase (const std::string &caseName, int32_t caseValue) | |
| Constructor. More... | |
| UnionCase (int32_t caseValue) | |
| Constructor. More... | |
| UnionCase (const std::string &caseName) | |
| Constructor. More... | |
| void | setUnionReferencePointer (UnionType *unionType) |
| This function set reference to union type. More... | |
| int32_t | getCaseValue () const |
| This function returns union case value. More... | |
| std::string | getCaseName () |
| This function returns union case name. More... | |
| std::vector< std::string > | getMemberDeclarationNames () const |
| This function returns vector of member declarations. More... | |
| void | addCaseMemberName (const std::string &name) |
| This function adds case member name. More... | |
| void | printUnionMembers () |
| This function prints debug information about union case members. | |
| bool | caseMemberIsVoid () const |
| This function returns information if case is void type. More... | |
| virtual std::string | getDescription () const |
| This function returns description about case members. More... | |
| StructMember * | getUnionMemberDeclaration (const std::string &name) |
| This function returns union member declaration. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| virtual bool | isBuiltin () const |
| This function return "false" value as default for identify builtin type. More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (std::string name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (std::string name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (std::string comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (std::string comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Additional Inherited Members | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol, kAliasTypeSymbol, kArrayTypeSymbol, kBuiltinTypeSymbol, kEnumTypeSymbol, kFunctionTypeSymbol, kListTypeSymbol, kStructTypeSymbol, kUnionTypeSymbol } |
| Supported symbol types. | |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Discriminated union case type.
|
inline |
Constructor.
This function set symbol to union case and name to given name. It will also set case value.
| [in] | caseName | Given case name. |
| [in] | caseValue | Given case value. |
|
inline |
Constructor.
This function set symbol to union case. It will also set case value.
| [in] | caseValue | Given case value. |
|
inline |
Constructor.
This function set symbol to union case and name to given name. It will also set case value to -1 (unset).
| [in] | caseName | Given case name. |
|
inline |
This function adds case member name.
param[in] name Case member name.
| bool UnionCase::caseMemberIsVoid | ( | ) | const |
This function returns information if case is void type.
| true | When case is void type. |
| false | When case contains not void type. |
|
inline |
This function returns union case name.
|
inline |
This function returns union case value.
|
virtual |
This function returns description about case members.
Reimplemented from erpcgen::Symbol.
|
inline |
This function returns vector of member declarations.
| StructMember * UnionCase::getUnionMemberDeclaration | ( | const std::string & | name | ) |
This function returns union member declaration.
param[in] name Union member name.
|
inline |
This function set reference to union type.
| [in] | unionType | Pointer to union type. |