![]() |
RPMsg-Lite User's Guide
Rev. 3.1.0
NXP Semiconductors
|
This section describes the RPMsg-Lite core component that allows: More...
This section describes the RPMsg-Lite core component that allows:
Classes | |
| struct | rpmsg_lite_endpoint |
| struct | rpmsg_lite_ept_static_context |
| struct | rpmsg_lite_instance |
Macros | |
| #define | RL_VERSION |
| #define | RL_WORD_SIZE |
| #define | RL_WORD_ALIGN_UP(a) |
| #define | RL_WORD_ALIGN_DOWN(a) |
| #define | RL_SUCCESS |
| #define | RL_NULL |
| #define | RL_REMOTE |
| #define | RL_MASTER |
| #define | RL_TRUE |
| #define | RL_FALSE |
| #define | RL_ADDR_ANY |
| #define | RL_RELEASE |
| #define | RL_HOLD |
| #define | RL_DONT_BLOCK |
| #define | RL_BLOCK |
| #define | RL_ERRORS_BASE |
| #define | RL_ERR_NO_MEM |
| #define | RL_ERR_BUFF_SIZE |
| #define | RL_ERR_PARAM |
| #define | RL_ERR_DEV_ID |
| #define | RL_ERR_MAX_VQ |
| #define | RL_ERR_NO_BUFF |
| #define | RL_NOT_READY |
| #define | RL_ALREADY_DONE |
| #define | RL_NO_FLAGS |
Typedefs | |
| typedef int32_t(* | rl_ept_rx_cb_t) (void *payload, uint32_t payload_len, uint32_t src, void *priv) |
| Receive callback function type. | |
Functions | |
| struct rpmsg_lite_instance * | rpmsg_lite_master_init (void *shmem_addr, size_t shmem_length, uint32_t link_id, uint32_t init_flags) |
| Initializes the RPMsg-Lite communication stack. Must be called prior to any other RPMSG lite API. To be called by the master side. More... | |
| struct rpmsg_lite_instance * | rpmsg_lite_remote_init (void *shmem_addr, uint32_t link_id, uint32_t init_flags) |
| Initializes the RPMsg-Lite communication stack. Must be called prior to any other RPMsg-Lite API. To be called by the remote side. More... | |
| int32_t | rpmsg_lite_deinit (struct rpmsg_lite_instance *rpmsg_lite_dev) |
| Deinitialized the RPMsg-Lite communication stack This function always succeeds. rpmsg_lite_init() can be called again after this function has been called. More... | |
| struct rpmsg_lite_endpoint * | rpmsg_lite_create_ept (struct rpmsg_lite_instance *rpmsg_lite_dev, uint32_t addr, rl_ept_rx_cb_t rx_cb, void *rx_cb_data) |
| Create a new rpmsg endpoint, which can be used for communication. More... | |
| int32_t | rpmsg_lite_destroy_ept (struct rpmsg_lite_instance *rpmsg_lite_dev, struct rpmsg_lite_endpoint *rl_ept) |
| This function deletes rpmsg endpoint and performs cleanup. More... | |
| int32_t | rpmsg_lite_send (struct rpmsg_lite_instance *rpmsg_lite_dev, struct rpmsg_lite_endpoint *ept, uint32_t dst, char *data, uint32_t size, uint32_t timeout) |
| Sends a message contained in data field of length size to the remote endpoint with address dst. ept->addr is used as source address in the rpmsg header of the message being sent. More... | |
| int32_t | rpmsg_lite_is_link_up (struct rpmsg_lite_instance *rpmsg_lite_dev) |
| Function to get the link state. More... | |
| int32_t | rpmsg_lite_release_rx_buffer (struct rpmsg_lite_instance *rpmsg_lite_dev, void *rxbuf) |
| Releases the rx buffer for future reuse in vring. This API can be called at process context when the message in rx buffer is processed. More... | |
| void * | rpmsg_lite_alloc_tx_buffer (struct rpmsg_lite_instance *rpmsg_lite_dev, uint32_t *size, uint32_t timeout) |
| Allocates the tx buffer for message payload. More... | |
| int32_t | rpmsg_lite_send_nocopy (struct rpmsg_lite_instance *rpmsg_lite_dev, struct rpmsg_lite_endpoint *ept, uint32_t dst, void *data, uint32_t size) |
| Sends a message in tx buffer allocated by rpmsg_lite_alloc_tx_buffer() More... | |
| struct rpmsg_lite_endpoint |
RPMsg Lite Endpoint structure
| Class Members | ||
|---|---|---|
| uint32_t | addr |
endpoint address |
| rl_ept_rx_cb_t | rx_cb |
ISR callback function |
| void * | rx_cb_data |
ISR callback data |
| void * | rfu |
reserved for future usage |
| struct rpmsg_lite_ept_static_context |
RPMsg Lite Endpoint static context
| Class Members | ||
|---|---|---|
| struct rpmsg_lite_endpoint | ept |
memory for endpoint structure |
| struct llist | node |
memory for linked list node structure |
| struct rpmsg_lite_instance |
Structure describing the local instance of RPMSG lite communication stack and holds all runtime variables needed internally by the stack.
| #define RL_VERSION |
Current RPMsg Lite version
| struct rpmsg_lite_instance* rpmsg_lite_master_init | ( | void * | shmem_addr, |
| size_t | shmem_length, | ||
| uint32_t | link_id, | ||
| uint32_t | init_flags | ||
| ) |
Initializes the RPMsg-Lite communication stack. Must be called prior to any other RPMSG lite API. To be called by the master side.
| shmem_addr | Shared memory base used for this instance of RPMsg-Lite |
| shmem_length | Length of memory area given by previous parameter |
| link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h |
| init_flags | Initialization flags |
| env_cfg | Initialization data for the environement RPMsg-Lite layer, used when the environment layer uses its own context (RL_USE_ENVIRONMENT_CONTEXT) |
| static_context | RPMsg-Lite preallocated context pointer, used in case of static api (RL_USE_STATIC_API) |
| struct rpmsg_lite_instance* rpmsg_lite_remote_init | ( | void * | shmem_addr, |
| uint32_t | link_id, | ||
| uint32_t | init_flags | ||
| ) |
Initializes the RPMsg-Lite communication stack. Must be called prior to any other RPMsg-Lite API. To be called by the remote side.
| shmem_addr | Shared memory base used for this instance of RPMsg-Lite |
| link_id | Link ID used to define the rpmsg-lite instance, see rpmsg_platform.h |
| init_flags | Initialization flags |
| env_cfg | Initialization data for the environement RPMsg-Lite layer, used when the environment layer uses its own context (RL_USE_ENVIRONMENT_CONTEXT) |
| static_context | RPMsg-Lite preallocated context pointer, used in case of static api (RL_USE_STATIC_API) |
| int32_t rpmsg_lite_deinit | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev | ) |
Deinitialized the RPMsg-Lite communication stack This function always succeeds. rpmsg_lite_init() can be called again after this function has been called.
| rpmsg_lite_dev | RPMsg-Lite instance |
| struct rpmsg_lite_endpoint* rpmsg_lite_create_ept | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| uint32_t | addr, | ||
| rl_ept_rx_cb_t | rx_cb, | ||
| void * | rx_cb_data | ||
| ) |
Create a new rpmsg endpoint, which can be used for communication.
| rpmsg_lite_dev | RPMsg-Lite instance |
| addr | Desired address, RL_ADDR_ANY for automatic selection |
| rx_cb | Callback function called on receive |
| rx_cb_data | Callback data pointer, passed to rx_cb |
| ept_context | Endpoint preallocated context pointer, used in case of static api (RL_USE_STATIC_API) |
| int32_t rpmsg_lite_destroy_ept | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| struct rpmsg_lite_endpoint * | rl_ept | ||
| ) |
This function deletes rpmsg endpoint and performs cleanup.
| rpmsg_lite_dev | RPMsg-Lite instance |
| rl_ept | Pointer to endpoint to destroy |
| int32_t rpmsg_lite_send | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| struct rpmsg_lite_endpoint * | ept, | ||
| uint32_t | dst, | ||
| char * | data, | ||
| uint32_t | size, | ||
| uint32_t | timeout | ||
| ) |
Sends a message contained in data field of length size to the remote endpoint with address dst. ept->addr is used as source address in the rpmsg header of the message being sent.
| rpmsg_lite_dev | RPMsg-Lite instance |
| ept | Sender endpoint |
| dst | Remote endpoint address |
| data | Payload buffer |
| size | Size of payload, in bytes |
| timeout | Timeout in ms, 0 if nonblocking |
| int32_t rpmsg_lite_is_link_up | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev | ) |
Function to get the link state.
| rpmsg_lite_dev | RPMsg-Lite instance |
| int32_t rpmsg_lite_release_rx_buffer | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| void * | rxbuf | ||
| ) |
Releases the rx buffer for future reuse in vring. This API can be called at process context when the message in rx buffer is processed.
| rpmsg_lite_dev | RPMsg-Lite instance |
| rxbuf | Rx buffer with message payload |
| void* rpmsg_lite_alloc_tx_buffer | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| uint32_t * | size, | ||
| uint32_t | timeout | ||
| ) |
Allocates the tx buffer for message payload.
This API can only be called at process context to get the tx buffer in vring. By this way, the application can directly put its message into the vring tx buffer without copy from an application buffer. It is the application responsibility to correctly fill the allocated tx buffer by data and passing correct parameters to the rpmsg_lite_send_nocopy() function to perform data no-copy-send mechanism.
| rpmsg_lite_dev | RPMsg-Lite instance | |
| [in] | size | Pointer to store maximum payload size available |
| [in] | timeout | Integer, wait upto timeout ms or not for buffer to become available |
| int32_t rpmsg_lite_send_nocopy | ( | struct rpmsg_lite_instance * | rpmsg_lite_dev, |
| struct rpmsg_lite_endpoint * | ept, | ||
| uint32_t | dst, | ||
| void * | data, | ||
| uint32_t | size | ||
| ) |
Sends a message in tx buffer allocated by rpmsg_lite_alloc_tx_buffer()
This function sends txbuf of length len to the remote dst address, and uses ept->addr as the source address. The application has to take the responsibility for:
After the rpmsg_lite_send_nocopy() function is issued the tx buffer is no more owned by the sending task and must not be touched anymore unless the rpmsg_lite_send_nocopy() function fails and returns an error.
| rpmsg_lite_dev | RPMsg-Lite instance | |
| [in] | ept | Sender endpoint pointer |
| [in] | dst | Destination address |
| [in] | data | TX buffer with message filled |
| [in] | size | Length of payload |