![]() |
RPMsg-Lite User's Guide
Rev. 3.1.0
NXP Semiconductors
|
#include "rpmsg_config.h"Go to the source code of this file.
Macros | |
| #define | RL_USE_CUSTOM_CONFIG |
Configuration options | |
| #define | RL_MS_PER_INTERVAL |
| #define | RL_BUFFER_PAYLOAD_SIZE |
| #define | RL_BUFFER_COUNT |
| #define | RL_API_HAS_ZEROCOPY |
| #define | RL_USE_STATIC_API |
| #define | RL_CLEAR_USED_BUFFERS |
| #define | RL_USE_MCMGR_IPC_ISR_HANDLER |
| #define | RL_USE_ENVIRONMENT_CONTEXT |
| #define | RL_DEBUG_CHECK_BUFFERS |
| #define | RL_ASSERT_BOOL(b) |
| #define | RL_ASSERT(x) |