Overview
========
The i2c_interrupt_b2b_transfer_slave example shows how to use i2c driver as slave to do board to board transfer 
with interrupt:

In this example, one i2c instance as slave and another i2c instance on the other board as master. Master sends a 
piece of data to slave, and receive a piece of data from slave. This example checks if the data received from 
slave is correct.

Toolchain supported
===================
- IAR embedded Workbench  8.50.5
- Keil MDK  5.31
- MCUXpresso  11.2.0
- GCC ARM Embedded  9.2.1

Hardware requirements
=====================
- Micro USB cable
- Two LPCXpresso51U68 boards
- Personal Computer

Board settings
==============
I2C one board:
  + Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C4 pins of MASTER_BOARD are connected with
    I2C4 pins of SLAVE_BOARD
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J1-1               I2C_SCL    J1-1
I2C_SDA    J1-3               I2C_SDA    J1-3
GND        J1-7               GND        J1-7
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Prepare the Demo
================
1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J6) on the board.
2. Open a serial terminal on PC for JLink serial device with these settings:
   - 115200 baud rate
   - 8 data bits
   - No parity
   - One stop bit
   - No flow control
3. Download the program to the target board.
4. Either press the reset button on your board or launch the debugger in your IDE to begin running
   the demo.

Running the demo
================
The following message shows in the terminal if the example runs successfully.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~
I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .
~~~~~~~~~~~~~~~~~~~~~~~~~~~~