Overview
========
The LED Blinky demo application provides a sanity check for the new SDK build environments and board bring up. The LED Blinky demo 
uses the systick interrupt to realize the function of timing delay. The example takes turns to shine the LED. The purpose of this 
demo is to provide a simple project for debugging and further development.
The code of this demo has been prepared and updated for use with the MCUXpresso Configuration Tools (Pins/Clocks/Peripherals).

Toolchain supported
===================
- IAR embedded Workbench  9.10.2
- Keil MDK  5.34
- MCUXpresso  11.4.0
- GCC ARM Embedded  10.2.1

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso54S018 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
2.  Download the program to the target board.

Running the demo
================
When the demo runs successfully, you will find the LED is blinking.