Overview
========
The Hello World project is a simple demonstration program that uses the SDK UART drivere in
combination with FreeRTOS. The purpose of this demo is to show how to use the debug console and to
provide a simple project for debugging and further development.

The example application creates one task called hello_task. This task print "Hello world." message
via debug console utility and suspend itself.




Toolchain supported
===================
- IAR embedded Workbench  8.50.6
- GCC ARM Embedded  9.2.1

Hardware requirements
=====================
- Micro USB cable
- EVK-MIMX8M Plus board
- J-Link Debug Probe
- 12V power supply
- Personal Computer

Board settings
==============
No special settings are required.



Prepare the Demo
================
1.  Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board
2.  Connect a USB cable between the host PC and the J23 USB port on the target board.
3.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
4.  Download the program to the target board.
5.  Launch the debugger in your IDE to begin running the demo.

Running the demo
================
After the board is flashed the Tera Term will print "Hello world" message on terminal.

Example output:
Hello world.