Overview
========
The IPED Example project is a demonstration program that uses the MCUX SDK software to set up Inline Prince Encryption Decryption.
Then tests the expected behaviour.


Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============
 Connect pin 1-2 of JP41,JP42,JP43 ,JP44,JP45,JP64 and JP65.Close JP66,JP67,JP68 and JP69.

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
When the demo runs successfully, the terminal displays similar information like the following:
~~~~~~~~~~~~~~~~~~
IPED Peripheral Driver Example

Calling API_Init
API_Init Successfully
Configure IPED region 0 enc/dec: start 0x8002000 end 0x8003000
Configure IPED  Successfully
External Flash memory configured successfully
*Success* read plain data from 0x8001000 to 0x8001FFF
*Success* read programmed&encrypted data from 0x08002000 to 0x8002FFF
*Success* read plain data from 0x8003000 to 0x8003FFF
Disabling IPED
*Success* read plain data from 0x8001000 to 0x8001FFF
*Success* read encrypted data from 0x8002000 to 0x8002FFF
*Success* read plain data from 0x8003000 to 0x8003FFF
Enabling IPED
*Success* read plain data from 0x8001000 to 0x8001FFF
*Success* read decrypted data from 0x8002000 to 0x8002FFF
*Success* read plain data from 0x8003000 to 0x8003FFF
Reconfiguring IPED
Reconfigure IPED  Successfully
*Success* read plain data from 0x8001000 to 0x8001FFF
*Success* read decrypted data from 0x8002000 to 0x8002FFF
*Success* read plain data from 0x8003000 to 0x8003FFF
Disabling IPED
End of example

~~~~~~~~~~~~~~~~~~

Note: Please make sure that flash is cleared and a power cycle has been performed before executing.