Overview
========

The lpadc_polling example shows the simplest way to use LPADC driver.

In this example, user should indicate a channel to provide a voltage signal (can be controlled by user) as the LPADC's
sample input. When running the project, typing any key into debug console would trigger the conversion. The execution 
would check the FIFO valid flag in loop until the flag is asserted, which means the conversion is completed. 
Then read the conversion result value and print it to debug console.

Note, the default setting of initialization for the ADC converter is just an available configuration. User can change
the configuration structure's setting in application to fit the special requirement.


Toolchain supported
===================
- IAR embedded Workbench  9.40.1
- Keil MDK  5.38.1
- GCC ARM Embedded  12.2
- MCUXpresso  11.8.0

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S36 board
- Personal Computer

Board settings
==============
- ADC CH0A input signal J7-1(PIO1_9).

Prepare the Demo
================
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the hello world demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
LPADC Polling Example
ADC Full Range: 65536
Please press any key to get user channel's ADC value.
ADC value: 35596
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~