################################################################################
 Secure Boot - Getting Started
################################################################################

################################################################################
 Requirements
################################################################################
Hardware:
    - LPC55S36-EVK, Rev. D or newer, with the LPC55S36 A1 chip.
    - USB cable.

Software and Tools:
    - Windows 10 platform, to execute batch scripts.
    - Keil Vision IDE v5.36 or higher. http://www2.keil.com/mdk5
    - MCUXpresso Secure Provisioning Tool (SEC) v6 https://nxp.com/mcuxpresso/secure, installed to the default C:\nxp\MCUX_Provi_v6\bin folder.

Please follow the step by step guide how to do an initial provisioning, and following firmware (FW) updates.

################################################################################
0. Preparation.
################################################################################
    - Build the TFM Secure Boot example:
        - Open the "<example>\tfm_secure_boot_s\mdk\tfm_secure_boot.uvmpw" workspace in the Keil Vision IDE.
        - Click on the "Batch Build" button in the "Build Toolbar". It starts building of the tfm_secure_boot_s and tfm_secure_boot_ns projects.
        - Wait until all builds processes are finished.
          NOTE: The output files, which will be used for the Firmware (FW) image creation:
                - "<example>\tfm_secure_boot_s\mdk\release\tfm_secure_boot_s.hex".
                - "<example>\tfm_secure_boot_ns\mdk\release\tfm_secure_boot_ns.hex".

################################################################################
1. Provisioning.
################################################################################
    The provisioning should be performed only once.
    - Put the device to the In System Programming (ISP) mode:
        - Keep the jumper J43 ISP0 (1-2) open, whereas keep the jumper J43 ISP1 (3-4) close. It enables Auto ISP boot mode.
        - Connect a micro USB cable between the PC host and the FS USB J3 connector. After that, the device boots into the USB HID ISP mode.
		NOTE: Change the default setting of JP46 from 2-3 to 1-2, otherwise ISP via the FS USB J3 will not work.
    - Execute the "<example>\scripts\1_provision.bat" file.
      It performs a generation and a following loading of a provisioning SB file containing a CUST_MK_SK key, a Boot Image, a CMPA and CFPA images.
    - The provisioning scrip will ask you:  "Do you want to change the device Life Cycle (irreversible operation) [N,Y]?". 
      Possible answers:
        - Y = switch to the OEM_SECURE (In-field) state. It is irreversible and CMPA area will be locked. 
              You have 10 seconds to answer Y, otherwise the default answer is N.
        - N = do not change the life-cycle, so you can perform the provisioning many times.
              It is possible to switch the life-cycle later, by repeating the provisioning, or execute the "<example>\scripts\steps\1_3_seal_irreversible.bat" step.
    - The command log:
        ********************
        *** PROVISIONING ***
        ********************
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488065 (0x4b030101)
        Current Version = K3.1.1
        ### Flash erase. ###
        Response status = 0 (0x0) Success.
        SUCCESS
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488065 (0x4b030101)
        Current Version = K3.1.1
        ### Merge S and NS images to one input\tfm_secureboot.bin file ###
        ### Create CFPA page - binary ###
        pfr generate-binary -c configs\cfpa.json -o configs\cfpa.bin
        WARNING:spsdk.pfr.pfr:The configuration file doesn't contains silicon revision, the latest: '1a' has been used. (1991ms since start, pfr.py:372)
        Success. (PFR binary has been generated into configs\cfpa.bin.)
        ### Create CMPA page - binary ###
        pfr generate-binary -c configs\cmpa.json -e configs\mbi_config.json -o configs\cmpa.bin
        WARNING:spsdk.pfr.pfr:The configuration file doesn't contains silicon revision, the latest: '1a' has been used. (854ms since start, pfr.py:372)
        Success. (PFR binary has been generated into configs\cmpa.bin.)
        ### Create bootable image ###
        nxpimage mbi export configs\mbi_config.json
        Success. (Master Boot Image: C:/_ddm/KSDK/sdk_latest/mcu-sdk-2.0/boards/lpcxpresso55s36/tfm_examples/tfm_secureboot/scripts/spt_workspace/bootable_images/tfm_secureboot.bin created.)
        ### Create OEM SB file ###
        nxpimage sb31 export configs\sb3_config.json
        Success. (Secure binary 3.1: C:/_ddm/KSDK/sdk_latest/mcu-sdk-2.0/boards/lpcxpresso55s36/tfm_examples/tfm_secureboot/scripts/spt_workspace/bootable_images/tfm_secureboot.sb created.)
        ### Create Provisioning SB file [CUST-MK-SK] ###
        nxpdevhsm generate -u 0x1FC9,0x0025 -k configs\cust_mk_sk.bin -o configs\sb_seed.bin -f lpc55s3x bootable_images\dev_hsm_provisioning.sb
        "C:\nxp\MCUX_Provi_v6\bin\tools\spsdk\nxpdevhsm.exe"
         1: Initial target reset is disabled
         2: Generating OEM master share.
         3: Generating 48 bytes FW signing keys.
         4: Generating 48 bytes FW encryption keys.
         5: Wrapping user PCK key.
         6: Creating template un-encrypted SB3 header and data blobs.
         6.1: Creating template SB3 header.
         6.2: Creating un-encrypted SB3 data.
         7: Encrypting SB3 data on device
         7.1: Enriching encrypted SB3 data by mandatory hashes.
         7.2: Creating dummy certificate block.
         7.3: Updating SB3 header by valid values.
         7.4: Preparing SB3 manifest to sign.
         8: Creating SB3 manifest signature on device.
         9: Composing final SB3 file.
        10: Resetting the target device
        Final SB3 file has been written: C:\_ddm\KSDK\sdk_latest\mcu-sdk-2.0\boards\lpcxpresso55s36\tfm_examples\tfm_secureboot\scripts\spt_workspace\bootable_images\dev_hsm_provisioning.sb
        SUCCESS
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488065 (0x4b030101)
        Current Version = K3.1.1
        ### Write Provisioning SB file ###
        blhost -u 0x1FC9,0x0025 -- receive-sb-file bootable_images\dev_hsm_provisioning.sb
        Sending SB file  [####################################]  100%
        Response status = 0 (0x0) Success.
        ### Reset the processor, so the CUST_MK_SK key is applied ###
        Response status = 0 (0x0) Success.
        ### Write CFPA ###
        blhost -u 0x1FC9,0x0025 -- write-memory 0x0003DC00 configs\cfpa.bin
        Writing memory  [####################################]  100%
        Response status = 0 (0x0) Success.
        Response word 1 = 512 (0x200)
        ### Write CMPA ###
        blhost -u 0x1FC9,0x0025 -- write-memory 0x0003E200 configs\cmpa.bin
        Writing memory  [####################################]  100%
        Response status = 0 (0x0) Success.
        Response word 1 = 512 (0x200)
        ### Write OEM SB file ###
        blhost -u 0x1FC9,0x0025 -- receive-sb-file "bootable_images\tfm_secureboot.sb"
        Sending SB file  [####################################]  100%
        Response status = 0 (0x0) Success.
        SUCCESS
        WARNING: Do you want to change the device Life Cycle (irreversible operation) [N,Y]?Y
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488064 (0x4b030100)
        Current Version = K3.1.0
        ### Burn fuse: LC_STATE[7:0] ###
        Response status = 0 (0x0) Success.
        Response word 1 = True (0x1)
        SUCCESS
        *** Provisioning is SUCCESSFUL ***
        Press any key to continue . . .
    - Run the FW application according to the Chapter [4].
    NOTE:
          - To enable a secure debug authentication, update the CFPA area according to the Chapter [3]. 
          - The executable image is placed in the "<example>\scripts\spt_workspace\input\tfm_secureboot.bin" file.
            It is created by merging the "tfm_secure_boot_s.hex" and "tfm_secure_boot_ns.hex" files, by aligning it to 0x38000 (PRINCE region end) and folowing converting to the binary file.
          - The self-signed RoT authentication keys are located in "<example>\scripts\spt_workspace\keys\ROT<x>_p384.pem". First ROT1_p384.pem is used by default. 
          - The Customer Manufacturing Configuration Area (CMPA) configuration is located in the "<example>\scripts\spt_workspace\configs\cmpa.json" file:
             - Enables boot image authentication and integrity using ECDSA P-384 with SHA384.
             - Enables PRINCE-based memory encryption for [0x00000000-0x00037FFF] memory region to protect a FW confidentiality while the FW image is stored in the internal Flash.
             - Disables the Debug Interface.
             - Enforces CMAC checking of images (SECURE_BOOT_CFG[31:30] = 0b01 in the PFR).
               Even if this bit field is set during first boot of the application image,
               the ECDSA algorithm is always used to verify authenticity of the image. After successful authentication,
               the bootloader calculates CMAC over the whole image. Device specific CMAC key is used.
               Calculated CMAC is then stored in Protected Flash Region (PFR), so that it can be used for authentication during next boot.
         - The Customer In-field Programmable Area (CFPA) configuration is located in the "<example>\scripts\spt_workspace\configs\cfpa.json" file.
         - The Master Boot Image (MBI) configuration is located in the "<example>\scripts\spt_workspace\configs\mbi_config.json" file.
         - The CUST_MK_SK master key, to derive FW image encryption key, located in the "<example>\scripts\spt_workspace\cust_mk_sk.bin" file.
         - The OEM share input, to use as a seed to randomize the provisioning process, located in the "<example>\scripts\spt_workspace\sb_seed.bin" file.

################################################################################
2. Update firmware (FW).
################################################################################
    It is optional, as the provisioned device already contains the initial version of FW.
    The FW update can be performed only on an already provisioned device.
    - Put the device to the In System Programming (ISP) mode:
        - Keep the jumper J43 ISP0 (1-2) open, whereas keep the jumper J43 ISP1 (3-4) close. It enables Auto ISP boot mode.
        - Connect a micro USB cable between the PC host and the FS USB J3 connector. After that, the device boots into the USB HID ISP mode.
		NOTE: Change the default setting of JP46 from 2-3 to 1-2, otherwise ISP via the FS USB J3 will not work.
    - Execute the "<example>\scripts\2_update_fw.bat" file.
    - It performs generation and following loading of the OEM SB file containing the updated FW.
    - The command log:
        ********************
        **** FW UPDATE *****
        ********************
        ### Merge S and NS images to one input\tfm_secureboot.bin file ###
        ### Create bootable image ###
        nxpimage mbi export configs\mbi_config.json
        Success. (Master Boot Image: C:/_ddm/KSDK/sdk_latest/mcu-sdk-2.0/boards/lpcxpresso55s36/tfm_examples/tfm_secureboot/scripts/spt_workspace/bootable_images/tfm_secureboot.bin created.)
        ### Create OEM SB file ###
        nxpimage sb31 export configs\sb3_config.json
        Success. (Secure binary 3.1: C:/_ddm/KSDK/sdk_latest/mcu-sdk-2.0/boards/lpcxpresso55s36/tfm_examples/tfm_secureboot/scripts/spt_workspace/bootable_images/tfm_secureboot.sb created.)
        SUCCESS
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488064 (0x4b030100)
        Current Version = K3.1.0
        ### Update bootable image using SB file ###
        blhost -u 0x1FC9,0x0025 -- receive-sb-file "bootable_images\tfm_secureboot.sb"
        Sending SB file  [####################################]  100%
        Response status = 10203 (0x27db) Memory Cumulative Write.
        SUCCESS
        *** FW Update is SUCCESSFUL ***
        Press any key to continue . . .
    - Run the FW application according to the Chapter [4].
    NOTE:
        - The executable image is placed in the "<example>\scripts\spt_workspace\input\tfm_secureboot.bin" file.
          It is created by merging "tfm_secure_boot_s.hex" and "tfm_secure_boot_ns.hex" files, by aligning it to 0x38000 (PRINCE region end)
          and following converting to the binary file.
        - The Master Boot Image (MBI) configuration is located in the "<example>\scripts\spt_workspace\configs\mbi_config.json" file.
        - If the FW Secure Boot is failed, it goes to the ISP mode.

################################################################################
3. Update Customer In-field Programmable Area (CFPA).
################################################################################
    It is optional, the CFPA table should be reprogrammed only when a major change in the firmware version 
    is needed, when a change in security restrictions.
    The CFPA update can be performed only on an already provisioned device, described in the Chapter [1].
    - Put the device to the In System Programming (ISP) mode:
        - Keep the jumper J43 ISP0 (1-2) open, whereas keep the jumper J43 ISP1 (3-4) close. It enables Auto ISP boot mode.
        - Connect a micro USB cable between the PC host and the FS USB J3 connector. After that, the device boots into the USB HID ISP mode.
		NOTE: Change the default setting of JP46 from 2-3 to 1-2, otherwise ISP via the FS USB J3 will not work.
    - Execute the "<example>\scripts\3_update_cfpa.bat" file.
    - It performs a generation and following loading of the OEM SB file containing the CFPA page.
    - The command log:
        ********************
        *** CFPA UPDATE ****
        ********************
        ### Create CFPA binary ###
        pfr generate-binary -c configs\cfpa.json -o configs\cfpa.bin
        WARNING:spsdk.pfr.pfr:The configuration file doesn't contains silicon revision, the latest: '1a' has been used. (659ms since start, pfr.py:372)
        Success. (PFR binary has been generated into configs\cfpa.bin.)
        ### Create CFPA SB file ###
        nxpimage sb31 export configs\sb3_cfpa_config.json
        Success. (Secure binary 3.1: C:/_ddm/KSDK/sdk_latest/mcu-sdk-2.0/boards/lpcxpresso55s36/tfm_examples/tfm_secureboot/scripts/spt_workspace/bootable_images/tfm_secureboot_cfpa.sb created.)
        SUCCESS
        ### Check connection ###
        Response status = 0 (0x0) Success.
        Response word 1 = 1258488064 (0x4b030100)
        Current Version = K3.1.0
        ### Update Customer Field Programmable Area [CFPA] ###
        blhost -u 0x1FC9,0x0025 -- receive-sb-file "bootable_images\tfm_secureboot_cfpa.sb"
        Sending SB file  [####################################]  100%
        Response status = 0 (0x0) Success.
        SUCCESS
        *** CFPA Update is SUCCESSFUL ***
        Press any key to continue . . .
    - Run the FW application according to the Chapter [4].
    NOTE:
        - The CFPA configuration is located in the "<example>\scripts\spt_workspace\configs\cfpa.json" file.
        - If the CFPA Page Version is less than or equal to its current value, the CFPA update fails with the "FLASH Driver: Out Of Date CFPA Page" error message, .
          Increase the value of the "CFPA_PAGE_VERSION" field in the "<example>\scripts\spt_workspace\configs\cfpa.json" file
          or set it to 0xFFFFFFFF for the automatic CFPA veriosn incrementation.

################################################################################
4. Run FW application.
################################################################################
    To perform a secure boot of the device:
    - Disable the ISP mode, keep the J43 ISP0 (1-2) and ISP1 (3-4) jumpers open.
    - Connect a micro USB cable between the PC host and the CMSIS DAP USB port Link2 J1 connector on the board.
    - Determine serial port number of the connected device:
        - Open the Device Manager. Find the "LPC-LinkII UCom Port (COMx)" port number in the "Ports(COM & LPT)" folder. 
        - Use the COM port number for a serial terminal application.
    - Open a serial terminal for the determined COM port.
    - After power up, the device preforms the secure boot of the uploaded FW.
    - The serial terminal log:
        [WRN] This device was provisioned with dummy keys. This device is NOT SECURE
        [Sec Thread] Secure image initializing!
        TF-M Float ABI: Hard
        Lazy stacking enabled
        Booting TF-M 1.7.0
        Non-Secure system starting...
        
        ***** PSA Architecture Test Suite - Version 1.4 *****
        
        Running.. Crypto Suite
        ******************************************
        
        TEST: 201 | DESCRIPTION: Testing crypto key management APIs | UT:  psa_crypto_init
        [Info] Executing tests from non-secure
        [Check 1] Test calling crypto functions before psa_crypto_init
        [Check 2] Test psa_crypto_init
        [Check 3] Test multiple psa_crypto_init
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 202 | DESCRIPTION: Testing crypto key management APIs | UT: psa_import_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_import_key with EC Public key
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 203 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_export_key with EC Public key
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 204 | DESCRIPTION: Testing crypto key management APIs | UT: psa_export_public_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_export_public_key with EC Public key
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 205 | DESCRIPTION: Testing crypto key management APIs | UT: psa_destroy_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_destroy_key with EC Public key
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 206 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_compute
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_compute with SHA256 algorithm
        [Check 2] Test psa_hash_compute with invalid algorithm
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 207 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_compare
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_compare with SHA256 algorithm
        [Check 2] Test psa_hash_compare with incorrect hash
        [Check 3] Test psa_hash_compare with incorrect hash length
        [Check 4] Test psa_hash_compare with invalid algorithm
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 208 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_setup - ECDH + HKDF-SHA-256
        [Check 2] Test psa_key_derivation_setup - ECDH, unknown KDF
        [Check 3] Test psa_key_derivation_setup - bad key derivation algorithm
        [Check 4] Test psa_key_derivation_setup - Invalid Algorithm
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 209 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_input_bytes
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_input_bytes - Step as Info
        [Check 2] Test psa_key_derivation_input_bytes - Step as secret
        [Check 3] Test psa_key_derivation_input_bytes - Step as salt
        [Check 4] Test psa_key_derivation_input_bytes - Step as label
        [Check 5] Test psa_key_derivation_input_bytes - Step as seed
        [Check 6] Test psa_key_derivation_input_bytes - Invalid step
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 210 | DESCRIPTION: Testing crypto key attributes APIs | UT: psa_key_attributes_set_get
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_attributes_set_get key attributes
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 211 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_setup with SHA256 algorithm
        [Check 2] Test psa_hash_setup with Invalid hash algorithm
        [Check 3] Test psa_hash_setup with Invalid algorithm
        [Check 4] Test psa_hash_setup with CTR algorithm
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 212 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_update
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_update with SHA256 algorithm
        [Check 2] Test psa_hash_update without hash setup
        [Check 3] Test psa_hash_update with completed opertaion handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 213 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_verify
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_verify with SHA256 algorithm
        [Check 2] Test psa_hash_verify with incorrect expected hash
        [Check 3] Test psa_hash_verify with incorrect hash length
        [Check 4] test psa_hash_verify with inactive & invalid operation handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 214 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_finish
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_finish with SHA256 algorithm
        [Check 2] Test psa_hash_finish with invalid hash buffer size
        [Check 3] test psa_hash_finish with inactive operation handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 215 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_abort
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_abort with SHA256 algorithm
        [Check 2] Test psa_hash_finish after calling psa_hash_abort
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 216 | DESCRIPTION: Testing crypto generator functions APIs | UT: psa_generate_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_generate_key with invalid key type
        [Check 2] Test psa_generate_key with invalid usage flags
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 217 | DESCRIPTION: Testing crypto generation APIs | UT: psa_generate_random
        [Info] Executing tests from non-secure
        [Check 1] Test psa_generate_random to get 0 Byte data
        [Check 2] Test psa_generate_random to get 16 Byte data
        [Check 3] Test psa_generate_random to get 24 Byte data
        [Check 4] Test psa_generate_random to get 32 Byte data
        [Check 5] Test psa_generate_random to get 64 Byte data
        [Check 6] Test psa_generate_random to get 128 Byte data
        [Check 7] Test psa_generate_random to get 256 Byte data
        [Check 8] Test psa_generate_random to get 512 Byte data
        [Check 9] Test psa_generate_random to get 1000 Byte data
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 218 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_input_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_input_key 16 Byte Key
        [Check 2] Test psa_key_derivation_input_key with invalid usage
        [Check 3] Test psa_key_derivation_input_key with step as label
        [Check 4] Test psa_key_derivation_input_key with step as info
        [Check 5] Test psa_key_derivation_input_key with step as seed
        [Check 6] Test psa_key_derivation_input_key with step as salt
        [Check 7] Test psa_key_derivation_input_key with key type as AES(not derive)
        [Check 8] Test psa_key_derivation_input_key incorrect key algorithm
        [Check 9] Test psa_key_derivation_input_key with zero as step
        [Check 10] Test psa_cipher_decrypt_setup - Invalid key handle
        [Check 11] Test psa_cipher_decrypt_setup - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 219 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_key_agreement
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_key_agreement - KDF not a key agreement alg
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 220 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_output_bytes
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_output_bytes - HKDF
        [Check 2] Test psa_key_derivation_output_bytes - optional salt
        [Check 3] Test psa_key_derivation_output_bytes - capacity < output_length
        [Check 4] Test psa_key_derivation_output_bytes - missing info
        [Check 5] Test psa_key_derivation_output_bytes - missing salt/secret/info
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 221 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_output_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_output_key - Key
        [Check 2] Test psa_key_derivation_output_key - Info
        [Check 3] Test psa_key_derivation_output_key - Salt
        [Check 4] Test psa_key_derivation_output_key - Greater Capacity than available
        [Check 5] Test psa_key_derivation_output_key - ECC Public key
        [Check 6] Test psa_key_derivation_output_key -  ECC keypair (wrong key length)
        [Check 7] Test psa_key_derivation_output_key -  RSA Public Key[Check 8] Test psa_key_derivation_output_key -  RSA keypair
        [Check 9] Test psa_key_derivation_output_key - Invalid key size
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 222 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_abort
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_abort
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 223 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_key_derivation_set_get_capacity
        [Info] Executing tests from non-secure
        [Check 1] Test psa_key_derivation_set_get_capacity - < operation's capacity
        [Check 2] Test psa_key_derivation_set_get_capacity - = operation's capacity
        [Check 3] Test psa_key_derivation_set_get_capacity - > operation's capacity
        [Check 4] Test psa_key_derivation_set_get_capacity - unchanged capacity
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 224 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_encrypt
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_encrypt - CCM - AES - 13B nonce & 8B add data
        [Check 2] Test psa_aead_encrypt - CCM - AES - 13B nonce & 32B add data
        [Check 3] Test psa_aead_encrypt - CCM - AES - 24 bytes Tag length = 4
        [Check 4] Test psa_aead_encrypt - CCM - AES - Zero additional data
        [Check 5] Test psa_aead_encrypt - CCM - AES - Zero plaintext
        [Check 6] Test psa_aead_encrypt - Unsupported algorithm
        [Check 7] Test psa_aead_encrypt - Invalid usage flag
        [Check 8] Test psa_aead_encrypt - Invalid ciphertext_size
        [Check 9] Test psa_aead_encrypt - Invalid nonce
        [Check 10] Test psa_aead_encrypt - Invalid tag length 0
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 225 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_decrypt
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_decrypt - CCM - AES - 13B nonce & 8B add data
        [Check 2] Test psa_aead_decrypt - CCM - AES - 13B nonce & 32B add data
        [Check 3] Test psa_aead_decrypt - CCM - AES - 24 bytes Tag length = 4
        [Check 4] Test psa_aead_decrypt - CCM - AES - Zero additional data
        [Check 5] Test psa_aead_decrypt - CCM - AES - Zero plaintext
        [Check 6] Test psa_aead_decrypt - Unsupported algorithm
        [Check 7] Test psa_aead_decrypt - Invalid usage flag
        [Check 8] Test psa_aead_decrypt - Invalid plaintext_size
        [Check 9] Test psa_aead_decrypt - Invalid nonce
        [Check 10] Test psa_aead_decrypt - Invalid cihpertext
        [Check 11] Test psa_aead_decrypt - Invalid cihpertext_size
        [Check 12] Test psa_aead_decrypt - Invalid tag length 0
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 226 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_sign_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_sign_setup - HMAC - SHA256
        [Check 2] Test psa_mac_sign_setup - Invalid usage flag
        [Check 3] Test psa_mac_sign_setup - Invalid key type
        [Check 4] Test psa_mac_sign_setup - Truncated MAC too large
        [Check 5] Test psa_mac_sign_setup - Truncated MAC too small
        [Check 6] Test psa_mac_sign_setup - Unknown MAC algorithm
        [Check 7] Test psa_mac_sign_setup invalid key handle
        [Check 8] Test psa_mac_sign_setup zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 227 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_update
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_update - HMAC - SHA256 - 64 Byte
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 228 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_sign_finish
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_sign_finish  - HMAC - SHA256
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 229 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_verify_setup - HMAC - SHA256
        [Check 2] Test psa_mac_verify_setup - Invalid usage flag
        [Check 3] Test psa_mac_verify_setup - Invalid key type
        [Check 4] Test psa_mac_verify_setup - Truncated MAC too large
        [Check 5] Test psa_mac_verify_setup - Truncated MAC too small
        [Check 6] Test psa_mac_verify_setup - Unknown MAC algorithm
        [Check 7] Test psa_mac_verify_setup invalid key handle
        [Check 8] Test psa_mac_verify_setup zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 230 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify_finish
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_verify_finish - HMAC - SHA256
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 231 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_abort
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_abort - HMAC - SHA256
        [Check 2] Test psa_mac_sign_finish after calling psa_mac_abort
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 232 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_encrypt_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_cipher_encrypt_setup - unknown cipher algorithm
        [Check 2] Test psa_cipher_encrypt_setup - EC Public key
        [Check 3] Test psa_cipher_encrypt_setup - Invalid key handle
        [Check 4] Test psa_cipher_encrypt_setup - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 233 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_decrypt_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_cipher_decrypt_setup - unknown cipher algorithm
        [Check 2] Test psa_cipher_decrypt_setup - EC Public key
        [Check 3] Test psa_cipher_decrypt_setup - Invalid key handle
        [Check 4] Test psa_cipher_decrypt_setup - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 234 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_generate_iv
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 235 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_set_iv
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 236 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_update
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 237 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_finish
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 238 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_abort
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 239 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_encrypt
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 240 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_asymmetric_decrypt
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 241 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_sign_hash
        [Info] Executing tests from non-secure
        [Check 1] Test psa_sign_hash - ECDSA SECP256R1 SHA-256
        [Check 2] Test psa_sign_hash - Invalid key handle
        [Check 3] Test psa_sign_hash - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 242 | DESCRIPTION: Testing crypto asymmetric APIs | UT: psa_verify_hash
        [Info] Executing tests from non-secure
        [Check 1] Test psa_verify_hash - ECDSA KEY_PAIR SECP256R1 SHA-256
        [Check 2] Test psa_verify_hash - EC public key
        [Check 3] Test psa_verify_hash - Invalid key handle
        [Check 4] Test psa_verify_hash - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 243 | DESCRIPTION: Testing crypto key derivation APIs | UT: psa_raw_key_agreement
        [Info] Executing tests from non-secure
        [Check 1] Test psa_raw_key_agreement - Not a key agreement alg
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 244 | DESCRIPTION: Testing crypto key management APIs | UT: psa_copy_key
        [Info] Executing tests from non-secure
        [Check 1] Test psa_copy_key - EC Public key
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 245 | DESCRIPTION: Testing crypto hash functions APIs | UT: psa_hash_clone
        [Info] Executing tests from non-secure
        [Check 1] Test psa_hash_clone - SHA256 algorithm
        [Check 2] Test psa_hash_clone - from an inactive source operation
        [Check 3] Test psa_hash_clone - on an active target operation
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 246 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_compute
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_compute HMAC SHA 256
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 247 | DESCRIPTION: Testing crypto MAC APIs | UT: psa_mac_verify
        [Info] Executing tests from non-secure
        [Check 1] Test psa_mac_verify HMAC SHA 256
        [Check 2] Test psa_mac_verify - Incompactible HMAC for CMAC
        [Check 3] Test psa_mac_verify - Invalid usage
        [Check 4] Test psa_mac_verify - Truncated MAC too large
        [Check 5] Test psa_mac_verify - Truncated MAC too small
        [Check 6] Test psa_mac_verify - bad algorithm (unknown MAC algorithm)
        [Check 7] Test psa_mac_verify - Invalid key type
        [Check 8] Test psa_mac_verify small size buffer
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 248 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_encrypt
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 249 | DESCRIPTION: Testing crypto symmetric cipher APIs | UT: psa_cipher_decrypt
        [Info] Executing tests from non-secure
        No test available for the selected crypto configuration
        
        TEST RESULT: SKIPPED (Skip Code=0x2d)
        
        ******************************************
        
        TEST: 250 | DESCRIPTION: Testing crypto key management APIs | UT: psa_sign_message
        [Info] Executing tests from non-secure
        [Check 1] Test psa_sign_message - ECDSA SECP256R1 SHA-256
        [Check 2] Test psa_sign_message - Invalid key handle
        [Check 3] Test psa_sign_message - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 251 | DESCRIPTION: Testing crypto key management APIs | UT: psa_verify_message
        [Info] Executing tests from non-secure
        [Check 1] Test psa_verify_message - ECDSA KEY_PAIR SECP256R1 SHA-256
        [Check 2] Test psa_verify_message - ECDSA Public Key SECP256R1 SHA-256
        [Check 3] Test psa_verify_message - Invalid key handle
        [Check 4] Test psa_verify_message - Zero as key handle
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 252 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_encrypt_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_encrypt_setup - CCM - AES
        [Check 2] Test psa_aead_encrypt_setup - CCM - AES - Tag length = 4
        [Check 3] Test psa_aead_encrypt_setup - CCM - AES - Mismatched tag length
        [Check 4] Test psa_aead_encrypt_setup - CCM - AES - Default Tag length
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 253 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_decrypt_setup
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_decrypt_setup - CCM - AES
        [Check 2] Test psa_aead_decrypt_setup - CCM - AES - Tag length = 4
        [Check 3] Test psa_aead_decrypt_setup - CCM - AES - Mismatched tag length
        [Check 4] Test psa_aead_decrypt_setup - CCM - AES - Default Tag length
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 254 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_generate_nonce
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_generate_nonce - CCM
        [Check 2] Test psa_aead_generate_nonce - CCM - Tag length = 4
        [Check 3] Test psa_aead_generate_nonce - CCM - Small buffer size
        [Check 4] Test psa_aead_generate_nonce - CCM - Uninitialized operation
        [Check 5] Test psa_aead_generate_nonce - CCM - Decrypt operation
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 255 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_set_nonce
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_set_nonce - Encrypt - CCM
        [Check 2] Test psa_aead_set_nonce - Encrypt - CCM - Tag length = 4
        [Check 3] Test psa_aead_set_nonce - Encrypt - CCM - Small nonce size
        [Check 4] Test psa_aead_set_nonce - Encrypt - CCM - Large nonce size
        [Check 5] Test psa_aead_set_nonce - Encrypt - CCM - Invalid operation state
        [Check 6] Test psa_aead_set_nonce - Decrypt - CCM
        [Check 7] Test psa_aead_set_nonce - Decrypt - CCM - Tag length = 4
        [Check 8] Test psa_aead_set_nonce - Decrypt - CCM - Small nonce size
        [Check 9] Test psa_aead_set_nonce - Decrypt - CCM - Large nonce size
        [Check 10] Test psa_aead_set_nonce - Decrypt - CCM - Invalid operation state
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 256 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_set_lengths
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_set_lengths - Encrypt - CCM
        [Check 2] Test psa_aead_set_lengths - Encrypt - CCM - Tag length = 4
        [Check 3] Test psa_aead_set_lengths - Encrypt - CCM - Zero ad_length
        [Check 4] Test psa_aead_set_lengths - Encrypt - CCM - Zero plaintext_length
        [Check 5] Test psa_aead_set_lengths - Encrypt - CCM - Invalid operation state
        [Check 6] Test psa_aead_set_lengths - Decrypt - CCM
        [Check 7] Test psa_aead_set_lengths - Decrypt - CCM - Tag length = 4
        [Check 8] Test psa_aead_set_lengths - Decrypt - CCM - Zero ad_length
        [Check 9] Test psa_aead_set_lengths - Decrypt - CCM - Zero plaintext_length
        [Check 10] Test psa_aead_set_lengths - Decrypt - CCM - Invalid operation state
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 257 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_update_ad
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_update_ad - Encrypt - CCM
        [Check 2] Test psa_aead_update_ad - Encrypt - CCM - Tag length = 4
        [Check 3] Test psa_aead_update_ad - Encrypt - CCM - Zero ad_length
        [Check 4] Test psa_aead_update_ad - Encrypt - CCM - Zero plaintext_length
        [Check 5] Test psa_aead_update_ad - Encrypt - CCM - Invalid operation state
        [Check 6] Test psa_aead_update_ad - Encrypt - CCM - Overflow input length
        [Check 7] Test psa_aead_update_ad - Decrypt - CCM
        [Check 8] Test psa_aead_update_ad - Decrypt - CCM - Tag length = 4
        [Check 9] Test psa_aead_update_ad - Decrypt - CCM - Zero ad_length
        [Check 10] Test psa_aead_update_ad - Decrypt - CCM - Zero plaintext_length
        [Check 11] Test psa_aead_update_ad - Decrypt - CCM - Invalid operation state
        [Check 12] Test psa_aead_update_ad - Decrypt - CCM - Overflow input length
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 258 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_update
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_update - Encrypt - CCM
        [Check 2] Test psa_aead_update - Encrypt - CCM - Tag length = 4
        [Check 3] Test psa_aead_update - Encrypt - CCM - Zero ad_length
        [Check 4] Test psa_aead_update - Encrypt - CCM - Zero plaintext_length
        [Check 5] Test psa_aead_update - Encrypt - CCM - Small buffer size
        [Check 6] Test psa_aead_update - Encrypt - CCM - Less add data than specified
        [Check 7] Test psa_aead_update - Encrypt - CCM - Overflow input length
        [Check 8] Test psa_aead_update - Encrypt - CCM - Invalid operation state
        [Check 9] Test psa_aead_update - Decrypt - CCM
        [Check 10] Test psa_aead_update - Decrypt - CCM - Tag length = 4
        [Check 11] Test psa_aead_update - Decrypt - CCM - Zero ad_length
        [Check 12] Test psa_aead_update - Decrypt - CCM - Zero plaintext_length
        [Check 13] Test psa_aead_update - Decrypt - CCM - Small buffer size
        [Check 14] Test psa_aead_update - Decrypt - Less add data than specified
        [Check 15] Test psa_aead_update - Decrypt - CCM - Overflow input length
        [Check 16] Test psa_aead_update - Decrypt - CCM - Invalid operation state
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 259 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_finish
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_finish - AES-CCM
        [Check 2] Test psa_aead_finish - AES-CCM 24 bytes Tag length = 4
        [Check 3] Test psa_aead_finish - Small buffer size
        [Check 4] Test psa_aead_finish - Input length is less than plaintext length
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 260 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_abort
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_abort - Encrypt - CCM - AES
        [Check 2] Test psa_aead_abort - Decrypt - CCM - AES
        [Check 3] Test psa_aead_abort with all initializations
        
        TEST RESULT: PASSED
        
        ******************************************
        
        TEST: 261 | DESCRIPTION: Testing crypto AEAD APIs | UT: psa_aead_verify
        [Info] Executing tests from non-secure
        [Check 1] Test psa_aead_verify - AES-CCM
        [Check 2] Test psa_aead_verify - AES-CCM 24 bytes Tag length = 4
        [Check 3] Test psa_aead_verify - Small buffer size
        [Check 4] Test psa_aead_verify - Input length is less than plaintext length
        
        TEST RESULT: PASSED
        
        ******************************************
        
        ************ Crypto Suite Report **********
        TOTAL TESTS     : 61
        TOTAL PASSED    : 51
        TOTAL SIM ERROR : 0
        TOTAL FAILED    : 0
        TOTAL SKIPPED   : 10
        ******************************************
        
        Entering standby.. 

################################################################################
5. Debug FW application.
################################################################################
    To debug the firmware:
    - Run the FW application. Follow steps described in the Chapter 4.
    - Execute the "<example>\scripts\4_open_debug_port.bat" file, to perform a debug authentication and open the debug port on a device.
    - The command log:
        *********************
        ** Open Debug Port **
        *********************
           <...>

           <...>
        ### Debug Authentication ###
        nxpdebugmbox --protocol 2.1 auth --beacon 1 --certificate "debug_auth\debug_auth_cert.dc" --key "keys\debug_authentication_key_ECC_384.pem"
          #   Interface   Id              Description
        ------------------------------------------------------------------------------------------------
          0   PyOCD       ENMTTDPFS4PPI   NXP Semiconductors MCU-LINK on-board (r0C7) CMSIS-DAP V2.245
          #   Interface   Id              Description
        ------------------------------------------------------------------------------------------------
          0   PyOCD       ENMTTDPFS4PPI   NXP Semiconductors MCU-LINK on-board (r0C7) CMSIS-DAP V2.245
        The device is accessible for debugging.
        SUCCESS
        *** Debug Port Opening is SUCCESSFUL ***
    - Attach a debugger to the runing device and debug it. The debugger starts, and the target hardware stops at the current location of the program counter.
        - For Keil IDE:
            - Disable all of the following project options for a target:
                - Options For Target -> Debug - Load Application at startup.
                - Options For Target -> Debug -> Settings - Reset after connect.
                - Options For Target -> Utilities - Update Target before Debugging.
             - Start a Debug Session. The debugger starts withour the application loading and the hardware reset.
    NOTE:
          - If a device life-cycle has not been updated in OTP during provisioning, to test the debug authentication, the script is trying to update the life-cycle register.
          - The Debug Authentication Certificate is located in "<example>\scripts\spt_workspace\debug_auth\debug_auth_cert.dc".
          - The Debug Authentication Key is located in "<example>\scripts\spt_workspace\eys\debug_authentication_key_ECC_384.pem".

################################################################################
5. Factory mass erase.
################################################################################
    To do a mass erase of the whole flash memory including the Protected Flash Region (PFR):
    - Connect a micro USB cable between the PC host and the CMSIS DAP USB port Link2 J1 connector on the board.
    - Execute the "<example>\scripts\5_mass_erase.bat" file.
    - The command log:
        ********************
        * FLASH MASS ERASE *
        ********************
        ### Flash mass erase, including the Protected Flash Region. ###
          #   Interface   Id              Description
        ------------------------------------------------------------------------------------------------
          0   PyOCD       TC3WAGFJT4NLU   NXP Semiconductors MCU-LINK on-board (r0C3) CMSIS-DAP V2.245
        Mass flash erase succeeded
        SUCCESS
        *** Flash mass erase is SUCCESSFUL ***
        Press any key to continue . . .
    NOTE:
        - The Flash mass erase is available only if the device life-cycle has not been updated in OTP during the provisioning phase.

################################################################################
 Appendix.
################################################################################
- The scripts command configuration parameters are placed in the <example>\tfm_secureboot\scripts\config.cmd configuration file.
- The MCUXpresso Secure Provisioning Tool workspace is located in the "<example>\spt_workspace" folder, it can be used to change the CMPA, CFPA, PRINCE and MBI configurations.
- Useful documentation:
    - The Secure Provisioning SDK (SPSDK) user documentation: http://spsdk.nxp.com/index.html
    - The LPC55S3x Reference Manual, security chapters:
        - Secure Boot ROM.
        - Security features.
        - Life Cycle States.
        - Prince.
        - Intrusion and Tamper Response Controller (ITRC).
        - Crypto Sub System (CSS).
        - Public-Key Crypto Coprocessor (PKC).
        - Trusted Execution Environment
        - Physically Unclonable Function (PUF).
        - Code Watchdog Timer (CDOG).

*Copyright 2022-2023, NXP. All rights reserved.*