nxpCl.<component-name> begin with the prefix <component-name>_.nxpCl<Name> begin with the prefix NXPCL<NAME>_.nxpCl_.NXPCL_.In order to minimize CPU wait cycles during coprocessor activities, some CLNS functions (non-blocking functions) are implemented in a non-blocking way, which means that the underlying operation has not completed at function return.
It is the caller's responsibility to ensure that the operation has completed before further processing on the operation output data is performed.
The names of all non-blocking functions end with the suffix _Async.
The release consists of three files, the NXP Software Content Register softwareContentRegister.txt, the NXP Software License Agreement LICENSE.htm and an archive with the file name extension .zip. The archive contains the following data:
doc folder contains Doxygen HTML documentation of the CLNS interfaces and example code. Open doc/html/index.html in a browser to view its main page.examples folder contains integration example code for each included component.includes folder directly contains the header source files that make up the API of the CLNS.includes/platform folder contains platform-specific header files that are required for integration of the CLNS.static_library folder contains a static library (archive of object code files) that contains the CLNS binaries.LICENSE.htm file contains the NXP Software License Agreement.softwareContentRegister.txt file contains the NXP Software Content Register. Note that this file is identical to the softwareContentRegister.txt delivered alongside the archive.nxpClElsThis release of the CLNS is designed for compatibility with a specific version of the ELS hardware IP.
To identify that compatible version, see #NXPCLELS_HW_VERSION.
To identify your actual version of the ELS hardware IP at run-time, see #nxpClEls_GetHwVersion. For details about the ELS, read the document "Crypto Secure Sequencer – Reference Manual".
The base address of the ELS needs to be provided at runtime time using the symbol ip_css_base.
Example:
To optimize power utilization, the ELS hardware IP provides a clock gating mechanism to enable and disable itself. Prior to any ELS-based operations invoked via the CLNS, the ELS must be enabled. The CLNS API provides the following support functions to enable/disable the ELS hardware:
All input and output buffers of nxpClEls functions must be placed in memory regions that are accessible to the ELS hardware IP.
It is the caller's responsibility to ensure that the operation of a non-blocking function has completed before further processing on the operation output data is performed. For nxpClEls functions, this can be achieved by either polling the ELS hardware status flag or by acting on hardware interrupts. The CLNS implements the support functions #nxpClEls_WaitForOperation and #nxpClEls_LimitedWaitForOperation for the former method. #nxpClEls_WaitForOperation potentially waits an infinite amount of time, while #nxpClEls_LimitedWaitForOperation uses a counter to limit the amount of time spent waiting.
The ELS hardware IP contains a stand-alone Sha module which can be used in parallel with other ELS operations. ELS operations make use of a ELS-internal DMA (Direct Memory Access) module for data handling. The stand-alone Sha module is an exception of this behavior: It is the caller's responsibility to perform the data handling, which can be achieved using the CPU or the system DMA.
As for all other components, all input and output buffers of nxpClEls functions that store external keys must be CPU word-aligned. From a functional perspective, all other input and output buffers of nxpClEls functions have no alignment requirement, unless explicitly stated otherwise. Using CPU word-aligned buffers may improve operation performance.