Option values for mcuxClEls_CmacOption_t. More...
Macros | |
| #define | MCUXCLELS_CMAC_EXTERNAL_KEY_ENABLE |
| Set mcuxClEls_CmacOption_t.extkey to this value to use an external key. More... | |
| #define | MCUXCLELS_CMAC_EXTERNAL_KEY_DISABLE |
| Set mcuxClEls_CmacOption_t.extkey to this value to use a key from the ELS keystore. More... | |
| #define | MCUXCLELS_CMAC_INITIALIZE_DISABLE |
| Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk does not include the first block of the message. More... | |
| #define | MCUXCLELS_CMAC_INITIALIZE_ENABLE |
| Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk includes the first block of the message. More... | |
| #define | MCUXCLELS_CMAC_FINALIZE_DISABLE |
| Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk does not include the last block of the message. More... | |
| #define | MCUXCLELS_CMAC_FINALIZE_ENABLE |
| Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk includes the last block of the message. More... | |
Option values for mcuxClEls_CmacOption_t.
| #define MCUXCLELS_CMAC_EXTERNAL_KEY_ENABLE |
Set mcuxClEls_CmacOption_t.extkey to this value to use an external key.
| #define MCUXCLELS_CMAC_EXTERNAL_KEY_DISABLE |
Set mcuxClEls_CmacOption_t.extkey to this value to use a key from the ELS keystore.
| #define MCUXCLELS_CMAC_INITIALIZE_DISABLE |
Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk does not include the first block of the message.
| #define MCUXCLELS_CMAC_INITIALIZE_ENABLE |
Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk includes the first block of the message.
| #define MCUXCLELS_CMAC_FINALIZE_DISABLE |
Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk does not include the last block of the message.
| #define MCUXCLELS_CMAC_FINALIZE_ENABLE |
Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk includes the last block of the message.