Constants for mcuxClEls_EccSignOption_t and mcuxClEls_EccVerifyOption_t. More...
Macros | |
| #define | MCUXCLELS_ECC_VALUE_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the hash of the message. More... | |
| #define | MCUXCLELS_ECC_VALUE_NOT_HASHED |
| Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the plain message. More... | |
| #define | MCUXCLELS_ECC_VALUE_RTF |
| Set this option at mcuxClEls_EccSignOption_t.value to include the RTF in the signature, only for mcuxClEls_EccSignOption_t. More... | |
| #define | MCUXCLELS_ECC_VALUE_NO_RTF |
| Set this option at mcuxClEls_EccSignOption_t.value to not include the RTF in the signature, only for mcuxClEls_EccSignOption_t. More... | |
Constants for mcuxClEls_EccSignOption_t and mcuxClEls_EccVerifyOption_t.
| #define MCUXCLELS_ECC_VALUE_HASHED |
Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the hash of the message.
| #define MCUXCLELS_ECC_VALUE_NOT_HASHED |
Set this option at mcuxClEls_EccSignOption_t.value or mcuxClEls_EccVerifyOption_t.value to specify input is the plain message.
| #define MCUXCLELS_ECC_VALUE_RTF |
Set this option at mcuxClEls_EccSignOption_t.value to include the RTF in the signature, only for mcuxClEls_EccSignOption_t.
| #define MCUXCLELS_ECC_VALUE_NO_RTF |
Set this option at mcuxClEls_EccSignOption_t.value to not include the RTF in the signature, only for mcuxClEls_EccSignOption_t.