Defines all functions of mcuxClEls_Cipher. More...
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_Cipher_Async(mcuxClEls_CipherOption_t options |
| Performs AES encryption/decryption. More... | |
Variables | |
| MCUXCLELS_API mcuxClEls_KeyIndex_t | keyIdx |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const * | pKey |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t | keyLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const * | pInput |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t | inputLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t uint8_t * | pIV |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t uint8_t uint8_t * | pOutput |
Defines all functions of mcuxClEls_Cipher.
| MCUXCLELS_API MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClEls_Status_t | ) |
Performs AES encryption/decryption.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
Performs an AES encryption/decryption. Call #mcuxClEls_WaitForOperation to complete the operation.
| [in] | options | Encryption/decryption command options. For detailed information, see mcuxClEls_CipherOption_t. |
| [in] | keyIdx | Index of the key inside the ELS keystore. See parameter properties section in function description. |
| [in] | pKey | Memory area that contains the key. See parameter properties section in function description. |
| [in] | keyLength | Size of pKey in bytes. Must be a valid key size of MCUXCLELS_CIPHER_KEY_SIZE_AES_. See parameter properties section in function description. |
| [in] | pInput | Pointer to the input data to be encrypted/decrypted. Padding must be already applied. |
| [in] | inputLength | Size of pInput in bytes, must be a multiple of the block size. |
| [in,out] | pIV | A pointer to the memory location which contains/receives the IV/state of cipher. See parameter properties section in function description. |
| [out] | pOutput | Pointer to the output buffer to store encrypted/decrypted data. |
The properties of some parameters change with respect to selected options.
options.cphmde == MCUXCLELS_CIPHERPARAM_ALGORITHM_AES_ECB pIV is ignored.
options.cphmde == MCUXCLELS_CIPHERPARAM_ALGORITHM_AES_CBC pIV must be set to the IV (when encrypting the first block) or to the last block of the ciphertext of the previous operation. ELS will always read and write to this location.
options.cphsie is ignored.
@p options.cphsoe is ignored.</dd>
<dt>@p options.cphmde == #MCUXCLELS_CIPHERPARAM_ALGORITHM_AES_CTR</dt>
<dd>@p pIV must be set to the IV (when encrypting the first block) or to the state output of the previous
encryption/decryption operation. ELS will write to this location if @p options.cphsoe == #MCUXCLELS_CIPHER_STATE_OUT_ENABLE.</dd>
<dt>@p options.extkey == #MCUXCLELS_CIPHER_EXTERNAL_KEY</dt>
<dd>@p keyIdx is ignored.</dd>
<dt>@p options.extkey == #MCUXCLELS_CIPHER_INTERNAL_KEY</dt>
<dd>@p pKey is ignored.
@p keyLength is ignored.</dd>
| MCUXCLELS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLELS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLELS_STATUS_OK_WAIT | on successful request |