Defines all functions of mcuxClHash. More...
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClHash_Status_t) mcuxClHash_compute(mcuxClSession_Handle_t session | |
| One-shot Hash computation function. More... | |
Variables | |
| mcuxClHash_Algo_t | algorithm |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t | pIn |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t | inSize |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t | pOut |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t uint32_t *const | pOutSize |
| mcuxClHash_Context_t | pContext |
Defines all functions of mcuxClHash.
| MCUX_CSSL_FP_PROTECTED_TYPE | ( | mcuxClHash_Status_t | ) |
One-shot Hash computation function.
Deprecated type for mcuxClSession protected status codes.
Deprecated type for RSA protected status codes.
Deprecated type for error codes used by code-flow protected PKC component functions.
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Deprecated type for error codes used by code-flow protected Math component functions.
Deprecated type for Key component error codes, returned by functions with code-flow protection.
Deprecated type for ELS driver protected status codes.
Deprecated type for mcuxClEcc component return codes.
Multi-part Hash computation finalization function.
Multi-part Hash processing function.
Multi-part Hash initialization function.
This function performs a hash computation over the input message pIn, using the hash function provided by the algorithm input parameter, in one shot. Up to 2^32 bytes of data can be hashed with this function.
For example, to perform a SHA256 computation, the following needs to be provided:
The input parameter session has to be initialized by the function mcuxClSession_init prior to calling this function. (MCUXCL_FEATURE_SESSION_HAS_RTF)
| [in/out] | session Handle for the current CL session. | |
| [in] | algorithm | Hash algorithm that should be used during the computation. |
| [in] | pIn | Pointer to the input buffer that contains the data that needs to be hashed. |
| [in] | inSize | Number of bytes of data in the pIn buffer. |
| [out] | pOut | Pointer to the output buffer where the computed hash value is written. |
| [in/out] | pOutSize Will be incremented by the number of bytes of data that have been written to the pOut buffer. |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_FAILURE | Error occured during Hash operation |
| MCUXCLHASH_STATUS_INVALID_PARAMS | The provided function parameters do not fulfill requirements |
| MCUXCLHASH_STATUS_FAULT_ATTACK | A fault attack was detected |
This function performs the initialization for a multi-part hash operation.
| [in/out] | session Handle for the current CL session. | |
| [out] | pContext | Hash context which is used to maintain the state and store other relevant information about the operation. |
| [in] | algorithm | Hash algorithm that should be used during the computation operation. |
| MCUXCLHASH_STATUS_OK | Initialization successful |
| MCUXCLHASH_FAILURE | Error occurred during initialization function |
This function performs the processing of (a part of) a data stream for a Hash operation. The algorithm to be used will be determined based on the context that is provided.
| [in/out] | session Handle for the current CL session. | |
| [in/out] | pContext Hash context which is used to maintain the state and store other relevant information about the operation. | |
| [in] | pIn | Pointer to the input buffer that contains the data that needs to be processed. |
| [in] | inSize | Number of bytes of data in the pIn buffer. |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_FAILURE | Error occurred during Hash operation |
| MCUXCLHASH_STATUS_INVALID_PARAMS | The provided function parameters do not fulfill requirements |
| MCUXCLHASH_STATUS_FAULT_ATTACK | A fault attack was detected |
This function performs the finalization of a Hash computation operation. The algorithm to be used will be determined based on the context that is provided
| [in/out] | session Handle for the current CL session. | |
| [in/out] | pContext Hash context which is used to maintain the state and store other relevant information about the operation. | |
| [out] | pOut | Pointer to the output buffer where the computed hash value needs to be written. |
| [out] | pOutSize | Will be incremented by the number of bytes of data that have been written to the pOut buffer. |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_FAILURE | Error occurred during Hash operation |