Defines all types of the mcuxClHash component. More...
Typedefs | |
| typedef struct mcuxClHash_AlgorithmDescriptor | mcuxClHash_AlgorithmDescriptor_t |
| Hash mode/algorithm descriptor type. More... | |
| typedef const mcuxClHash_AlgorithmDescriptor_t *const | mcuxClHash_Algo_t |
| Hash mode/algorithm type. More... | |
| typedef struct mcuxClHash_ContextDescriptor | mcuxClHash_ContextDescriptor_t |
| Hash Context buffer type. More... | |
| typedef mcuxClHash_ContextDescriptor_t *const | mcuxClHash_Context_t |
| Hash Context type. More... | |
| typedef uint32_t | mcuxClHash_Status_t |
| Hash Status type. More... | |
Defines all types of the mcuxClHash component.
| typedef struct mcuxClHash_AlgorithmDescriptor mcuxClHash_AlgorithmDescriptor_t |
Hash mode/algorithm descriptor type.
This type captures all the information that the Hash interfaces need to know about a particular Hash mode/algorithm.
| typedef const mcuxClHash_AlgorithmDescriptor_t* const mcuxClHash_Algo_t |
Hash mode/algorithm type.
This type is used to refer to a Hash mode/algorithm.
| typedef struct mcuxClHash_ContextDescriptor mcuxClHash_ContextDescriptor_t |
Hash Context buffer type.
This type is used in the streaming interfaces to store the information about the current operation and the relevant internal state.
| typedef mcuxClHash_ContextDescriptor_t* const mcuxClHash_Context_t |
Hash Context type.
This type is used to refer to the Hash context.
| typedef uint32_t mcuxClHash_Status_t |
Hash Status type.
This type is used for hash return values: mcuxClHashStatusValues