Configuration options for the secure counter mechanism. More...
Macros | |
| #define | MCUX_CSSL_SC_USE_HYBRID_LOCAL_CDOG |
| If set to 1, use the hybrid secure counter mechanism implementation based on a SW counter stored in a local variable and the code watchdog (CDOG) HW IP block. More... | |
| #define | MCUX_CSSL_SC_USE_HW_CDOG |
| If set to 1, use the secure counter mechanism implementation based on the code watchdog (CDOG) HW IP block. More... | |
| #define | MCUX_CSSL_SC_USE_HW_SCM |
| If set to 1, use the secure counter mechanism implementation based on the subsystem control module (SCM) HW IP block. More... | |
| #define | MCUX_CSSL_SC_USE_HW_S3SCM |
| If set to 1, use the secure counter mechanism implementation based on the subsystem control module (S3SCM) HW IP block. More... | |
| #define | MCUX_CSSL_SC_USE_SW_LOCAL |
| If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a local variable. More... | |
| #define | MCUX_CSSL_SC_USE_SW_CONTEXT |
| If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a context structure. More... | |
| #define | MCUX_CSSL_SC_USE_SW_CALLBACK |
| If set to 1, use the secure counter mechanism implementation based on a SW counter pointed to through a callback function. More... | |
| #define | MCUX_CSSL_SC_USE_SW_GLOBAL |
| If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a global variable. More... | |
| #define | MCUX_CSSL_SC_USE_NONE |
| If set to 1, do not use the secure counter mechanism. More... | |
Configuration options for the secure counter mechanism.
| #define MCUX_CSSL_SC_USE_HYBRID_LOCAL_CDOG |
If set to 1, use the hybrid secure counter mechanism implementation based on a SW counter stored in a local variable and the code watchdog (CDOG) HW IP block.
| #define MCUX_CSSL_SC_USE_HW_CDOG |
If set to 1, use the secure counter mechanism implementation based on the code watchdog (CDOG) HW IP block.
| #define MCUX_CSSL_SC_USE_HW_SCM |
If set to 1, use the secure counter mechanism implementation based on the subsystem control module (SCM) HW IP block.
| #define MCUX_CSSL_SC_USE_HW_S3SCM |
If set to 1, use the secure counter mechanism implementation based on the subsystem control module (S3SCM) HW IP block.
| #define MCUX_CSSL_SC_USE_SW_LOCAL |
If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a local variable.
| #define MCUX_CSSL_SC_USE_SW_CONTEXT |
If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a context structure.
| #define MCUX_CSSL_SC_USE_SW_CALLBACK |
If set to 1, use the secure counter mechanism implementation based on a SW counter pointed to through a callback function.
| #define MCUX_CSSL_SC_USE_SW_GLOBAL |
If set to 1, use the secure counter mechanism implementation based on a SW counter stored in a global variable.
| #define MCUX_CSSL_SC_USE_NONE |
If set to 1, do not use the secure counter mechanism.