Type definitions of mcuxClEcc component. More...
#include <stdint.h>#include <mcuxClConfig.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClEcc_ParameterSizes.h>#include <mcuxClCore_Analysis.h>Go to the source code of this file.
Data Structures | |
| struct | mcuxClEcc_DomainParam_t |
| Parameter structure of elliptic curve of the form, y^2 = x^3 + a*x + b modulo prime p. More... | |
| struct | mcuxClEcc_KeyGen_Param_t |
| Parameter structure for function #mcuxClEcc_KeyGen. More... | |
| struct | mcuxClEcc_Sign_Param_t |
| Parameter structure for function #mcuxClEcc_Sign. More... | |
| struct | mcuxClEcc_Verify_Param_t |
| Parameter structure for function #mcuxClEcc_Verify. More... | |
| struct | mcuxClEcc_PointMult_Param_t |
| Parameter structure for function #mcuxClEcc_PointMult. More... | |
Macros | |
| #define | MCUXCLECC_STATUS_OK |
| Operation was successful. More... | |
| #define | MCUXCLECC_STATUS_INVALID_PARAMS |
| Parameters are invalid. More... | |
| #define | MCUXCLECC_STATUS_RNG_ERROR |
| Random number (DRBG / PRNG) error (unexpected behavior). More... | |
| #define | MCUXCLECC_STATUS_INVALID_SIGNATURE |
| ECDSA Signature is invalid. More... | |
| #define | MCUXCLECC_STATUS_NEUTRAL_POINT |
| The result of the point operation is the neutral point. More... | |
| #define | MCUXCLECC_STATUS_FAULT_ATTACK |
| Fault attack (unexpected behavior) is detected. More... | |
| #define | MCUXCLECC_STATUS_NOT_SUPPORTED |
| Functionality is not supported. More... | |
| #define | MCUXCLECC_STATUS_ERROR_SMALL_SUBGROUP |
| MONTDH public key lies in small subgroup. More... | |
| #define | mcuxClEcc_DomainParam_misc_Pack(byteLenN, byteLenP) |
| mcuxClEcc macros and defines to pack or access components of misc parameter of mcuxClEcc_DomainParam_t More... | |
| #define | mcuxClEcc_DomainParam_misc_byteLenP_offset |
| Offset of byteLenP in packed misc parameter of mcuxClEcc_DomainParam_t. More... | |
| #define | mcuxClEcc_DomainParam_misc_byteLenP_mask |
| Mask to extract byteLenP from packed misc parameter of mcuxClEcc_DomainParam_t. More... | |
| #define | mcuxClEcc_DomainParam_misc_byteLenN_offset |
| Offset of byteLenN in packed misc parameter of mcuxClEcc_DomainParam_t. More... | |
| #define | mcuxClEcc_DomainParam_misc_byteLenN_mask |
| Mask to extract byteLenN from packed misc parameter of mcuxClEcc_DomainParam_t. More... | |
| #define | mcuxClEcc_Sign_Param_optLen_Pack(byteLenHash) |
| mcuxClEcc macros and defines to pack or access components of optLen parameter of mcuxClEcc_Sign_Param_t More... | |
| #define | mcuxClEcc_Sign_Param_optLen_byteLenHash_offset |
| Offset of byteLenHash in packed optLen parameter of mcuxClEcc_Sign_Param_t. More... | |
| #define | mcuxClEcc_Sign_Param_optLen_byteLenHash_mask |
| Mask to extract byteLenHash from packed optLen parameter of mcuxClEcc_Sign_Param_t. More... | |
| #define | mcuxClEcc_Verify_Param_optLen_Pack(byteLenHash) |
| mcuxClEcc macros and defines to pack or access components of optLen parameter of mcuxClEcc_Verify_Param_t More... | |
| #define | mcuxClEcc_Verify_Param_optLen_byteLenHash_offset |
| Offset of byteLenHash in packed optLen parameter of mcuxClEcc_Verify_Param_t. More... | |
| #define | mcuxClEcc_Verify_Param_optLen_byteLenHash_mask |
| Mask to extract byteLenHash from packed optLen parameter of mcuxClEcc_Verify_Param_t. More... | |
Typedefs | |
| typedef uint32_t | mcuxClEcc_Status_t |
| Type for mcuxClEcc component return codes. More... | |
| typedef struct mcuxClEcc_MontDH_DomainParams | mcuxClEcc_MontDH_DomainParams_t |
| Type for MontDH domain parameters. More... | |
| typedef struct mcuxClEcc_EdDSA_DomainParams | mcuxClEcc_EdDSA_DomainParams_t |
| Type for EdDSA domain parameters. More... | |
| typedef struct mcuxClEcc_EdDSA_GenerateKeyPairDescriptor | mcuxClEcc_EdDSA_GenerateKeyPairDescriptor_t |
| EdDSA GenerateKeyPair variant descriptor type. More... | |
| typedef struct mcuxClEcc_EdDSA_SignatureProtocolDescriptor | mcuxClEcc_EdDSA_SignatureProtocolDescriptor_t |
| EdDSA SignatureProtocol variant descriptor type. More... | |
| typedef struct mcuxClEcc_Weier_DomainParams | mcuxClEcc_Weier_DomainParams_t |
| Type for Weierstrass ECC domain parameters. More... | |
Functions | |
| typedef | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEcc_Status_t) mcuxClEcc_Status_Protected_t |
| Deprecated type for mcuxClEcc component return codes. More... | |
Variables | |
| const mcuxClEcc_EdDSA_GenerateKeyPairDescriptor_t | mcuxClEcc_EdDsa_GeneratePrivKeyDescriptor |
| const mcuxClEcc_EdDSA_SignatureProtocolDescriptor_t | mcuxClEcc_EdDsa_Ed25519ProtocolDescriptor |
Type definitions of mcuxClEcc component.