ELS header for CMAC support. More...
Go to the source code of this file.
Data Structures | |
| union | mcuxClEls_CmacOption_t |
| Command option bit field for #mcuxClEls_Cmac_Async. More... | |
Macros | |
| #define | MCUXCLELS_CMAC_KEY_SIZE_128 |
| Size of 128 bit CMAC key (16 bytes) More... | |
| #define | MCUXCLELS_CMAC_KEY_SIZE_256 |
| Size of 256 bit CMAC key (32 bytes) More... | |
| #define | MCUXCLELS_CMAC_EXTERNAL_KEY_ENABLE |
| Set mcuxClEls_CmacOption_t.extkey to this value to use an external key. More... | |
| #define | MCUXCLELS_CMAC_EXTERNAL_KEY_DISABLE |
| Set mcuxClEls_CmacOption_t.extkey to this value to use a key from the ELS keystore. More... | |
| #define | MCUXCLELS_CMAC_INITIALIZE_DISABLE |
| Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk does not include the first block of the message. More... | |
| #define | MCUXCLELS_CMAC_INITIALIZE_ENABLE |
| Set mcuxClEls_CmacOption_t.initialize to this value if the message chunk includes the first block of the message. More... | |
| #define | MCUXCLELS_CMAC_FINALIZE_DISABLE |
| Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk does not include the last block of the message. More... | |
| #define | MCUXCLELS_CMAC_FINALIZE_ENABLE |
| Set mcuxClEls_CmacOption_t.finalize to this value if the message chunk includes the last block of the message. More... | |
| #define | MCUXCLELS_CMAC_OUT_SIZE |
Functions | |
| MCUXCLELS_API | MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClEls_Status_t) mcuxClEls_Cmac_Async(mcuxClEls_CmacOption_t options |
| Performs CMAC with AES-128 or AES-256. More... | |
Variables | |
| MCUXCLELS_API mcuxClEls_KeyIndex_t | keyIdx |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const * | pKey |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t | keyLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const * | pInput |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t | inputLength |
| MCUXCLELS_API mcuxClEls_KeyIndex_t uint8_t const size_t uint8_t const size_t uint8_t * | pMac |
ELS header for CMAC support.
This header exposes functions that enable using the ELS for the generation of cipher-based message authentication codes (CMAC). The supported cipher algorithm is AES-128 and AES-256.