Top-level API of the mcuxClHash component. More...
#include <mcuxClConfig.h>#include <mcuxClSession_Types.h>#include <mcuxClHash_Types.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClCore_Buffer.h>Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClHash_Status_t) mcuxClHash_compute(mcuxClSession_Handle_t session | |
| One-shot Hash computation function. More... | |
Variables | |
| mcuxClHash_Algo_t | algorithm |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t | pIn |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t | inSize |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t | pOut |
| mcuxClHash_Algo_t mcuxCl_InputBuffer_t uint32_t mcuxCl_Buffer_t uint32_t *const | pOutSize |
| mcuxClHash_Context_t | pContext |
Top-level API of the mcuxClHash component.