Type definitions for the mcuxClHash component. More...
#include <stdint.h>#include <stddef.h>#include <stdbool.h>#include <mcuxClConfig.h>#include <mcuxClSession_Types.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>Go to the source code of this file.
Typedefs | |
| typedef struct mcuxClHash_AlgorithmDescriptor | mcuxClHash_AlgorithmDescriptor_t |
| Hash mode/algorithm descriptor type. More... | |
| typedef const mcuxClHash_AlgorithmDescriptor_t *const | mcuxClHash_Algo_t |
| Hash mode/algorithm type. More... | |
| typedef struct mcuxClHash_ContextDescriptor | mcuxClHash_ContextDescriptor_t |
| Hash Context buffer type. More... | |
| typedef mcuxClHash_ContextDescriptor_t *const | mcuxClHash_Context_t |
| Hash Context type. More... | |
| typedef uint32_t | mcuxClHash_Status_t |
| Hash Status type. More... | |
Type definitions for the mcuxClHash component.