APIs of mcuxClMath component. More...
#include <mcuxClCore_Platform.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClPkc.h>#include <mcuxClSession.h>#include <mcuxClMath_Types.h>Go to the source code of this file.
Macros | |
| #define | MCUXCLMATH_SHIFTMODULUS(iNShifted, iN) |
| Helper macro for #mcuxClMath_ShiftModulus. More... | |
| #define | MCUXCLMATH_FP_SHIFTMODULUS(iNShifted, iN) |
| Helper macro for #mcuxClMath_ShiftModulus with flow protection. More... | |
| #define | MCUXCLMATH_NDASH(iN, iT) |
| Helper macro for #mcuxClMath_NDash. More... | |
| #define | MCUXCLMATH_FP_NDASH(iN, iT) |
| Helper macro for #mcuxClMath_NDash with flow protection. More... | |
| #define | MCUXCLMATH_QDASH(iQDash, iNShifted, iN, iT, len) |
| Helper macro for #mcuxClMath_QDash. More... | |
| #define | MCUXCLMATH_FP_QDASH(iQDash, iNShifted, iN, iT, len) |
| Helper macro for #mcuxClMath_QDash with flow protection. More... | |
| #define | MCUXCLMATH_QSQUARED(iQSqr, iNShifted, iN, iT) |
| Helper macro for #mcuxClMath_QSquared. More... | |
| #define | MCUXCLMATH_FP_QSQUARED(iQSqr, iNShifted, iN, iT) |
| Helper macro for #mcuxClMath_QSquared with flow protection. More... | |
| #define | MCUXCLMATH_MODINV(iR, iX, iN, iT) |
| Helper macro for #mcuxClMath_ModInv. More... | |
| #define | MCUXCLMATH_FP_MODINV(iR, iX, iN, iT) |
| Helper macro for #mcuxClMath_ModInv with flow protection. More... | |
| #define | MCUXCLMATH_REDUCEMODEVEN(iR, iX, iN, iT0, iT1, iT2, iT3) |
| Helper macro for #mcuxClMath_ReduceModEven. More... | |
| #define | MCUXCLMATH_FP_REDUCEMODEVEN(iR, iX, iN, iT0, iT1, iT2, iT3) |
| Helper macro for #mcuxClMath_ReduceModEven with flow protection. More... | |
| #define | MCUXCLMATH_MODEXP_SQRMULTL2R(pExp, byteLenExp, iR, iX, iN, iT) |
| Helper macro for #mcuxClMath_ModExp_SqrMultL2R. More... | |
| #define | MCUXCLMATH_FP_MODEXP_SQRMULTL2R(pExp, byteLenExp, iR, iX, iN, iT) |
| Helper macro for #mcuxClMath_ModExp_SqrMultL2R with flow protection. More... | |
| #define | MCUXCLMATH_SECMODEXP(session, pExp, pExpTemp, byteLenExp, iR, iX, iN, iTE, iT0, iT1, iT2, iT3) |
| Helper macro for #mcuxClMath_SecModExp. More... | |
| #define | MCUXCLMATH_SECMODEXP_WITHOUT_RERANDOMIZATION(session, pExp, pExpTemp, byteLenExp, iR, iX, iN, iTE, iT0, iT1, iT2, iT3) |
| Helper macro for #mcuxClMath_SecModExp with disabled operand re-randomization. More... | |
| #define | MCUXCLMATH_EXACTDIVIDEODD(iR, iX, iN, iT, xPkcByteLen, yPkcByteLen) |
| Helper macro for #mcuxClMath_ExactDivideOdd. More... | |
| #define | MCUXCLMATH_FP_EXACTDIVIDEODD(iR, iX, iN, iT, xPkcByteLen, yPkcByteLen) |
| Helper macro for #mcuxClMath_ExactDivideOdd with flow protection. More... | |
| #define | MCUXCLMATH_EXACTDIVIDE(iR, iX, iN, iT, xPkcByteLen, yPkcByteLen) |
| Helper macro for #mcuxClMath_ExactDivide. More... | |
| #define | MCUXCLMATH_FP_EXACTDIVIDE(iR, iX, iN, iT, xPkcByteLen, yPkcByteLen) |
| Helper macro for #mcuxClMath_ExactDivide with flow protection. More... | |
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (void) mcuxClMath_InitLocalUptrt(uint32_t i3_i2_i1_i0 | |
| Initializes and uses the new UPTRT and returns the address of original UPTRT. More... | |
| MCUX_CSSL_FP_PROTECTED_TYPE (uint32_t) mcuxClMath_TrailingZeros(uint8_t iX) | |
| Counts number of trailing zero bits of a PKC operand. More... | |
APIs of mcuxClMath component.