Memory header for set function. More...
Go to the source code of this file.
Macros | |
| #define | MCUXCLMEMORY_FP_MEMORY_SET(pTarget, val, byteLen) |
| Helper macro to call #mcuxClMemory_set with flow protection. More... | |
| #define | MCUXCLMEMORY_FP_MEMORY_SET_WITH_BUFF(pTarget, val, byteLen, buffLen) |
| Helper macro to call #mcuxClMemory_set with flow protection with buffer. More... | |
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (void) mcuxClMemory_set(uint8_t *pDst | |
| Sets all bytes of a memory buffer to a specified value. More... | |
Variables | |
| uint8_t | val |
| uint8_t size_t | length |
| uint8_t size_t size_t | bufLength |
Memory header for set function.
This header exposes functions that enable using memory set functions.