Top level APIs of mcuxClRandom component. More...
Go to the source code of this file.
Functions | |
| MCUX_CSSL_FP_PROTECTED_TYPE (mcuxClRandom_Status_t) mcuxClRandom_init(mcuxClSession_Handle_t pSession | |
| Random data generator initialization function. More... | |
Variables | |
| mcuxClRandom_Context_t | pContext |
| mcuxClRandom_Context_t mcuxClRandom_Mode_t | mode |
| uint8_t * | pOut |
| uint8_t uint32_t | outLength |
| uint32_t | securityStrength |
Top level APIs of mcuxClRandom component.