Example of using function mcuxClRsa_sign to perform the RSA signature generation primitive RSASP1 (private exponentiation and NO padding) according to PKCS #1 v2.2, using a key in plain format. More...
#include <mcuxClSession.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClPkc.h>#include <mcuxClRandom.h>#include <mcuxClRsa.h>#include <mcuxClToolchain.h>#include <mcuxClCore_Examples.h>#include <mcuxClEls.h>#include <mcuxClExample_ELS_Helper.h>Macros | |
| #define | RSA_KEY_BIT_LENGTH |
| The example uses a 1024-bit key. More... | |
| #define | RSA_KEY_BYTE_LENGTH |
| Converting the key-bitlength to bytelength. More... | |
Functions | |
| static const uint8_t modulus [RSA_KEY_BYTE_LENGTH] | __attribute__ ((aligned(4))) |
| Example value for public RSA modulus N. More... | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClRsa_sign_NoEncode_example) | |
| Performs a session set-up; a call to function mcuxClRsa_sign using mode mcuxClRsa_Mode_Verify_NoVerify; a session clean-up. More... | |
Example of using function mcuxClRsa_sign to perform the RSA signature generation primitive RSASP1 (private exponentiation and NO padding) according to PKCS #1 v2.2, using a key in plain format.
| #define RSA_KEY_BIT_LENGTH |
The example uses a 1024-bit key.
| #define RSA_KEY_BYTE_LENGTH |
Converting the key-bitlength to bytelength.
|
static |
Example value for public RSA modulus N.
Expected signature.
Input message.
Example value for private RSA exponent d.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClRsa_sign_NoEncode_example | ) |
Performs a session set-up; a call to function mcuxClRsa_sign using mode mcuxClRsa_Mode_Verify_NoVerify; a session clean-up.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |
Initialize ELS, Enable the ELS
Destroy Session and cleanup Session
Disable the ELS