Example of using function mcuxClRsa_verify to perform the RSA signature verification primitive RSAVP1 (public exponentiation and NO padding verification) according to PKCS #1 v2.2. More...
#include <mcuxClSession.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClPkc.h>#include <mcuxClRandom.h>#include <mcuxClRsa.h>#include <mcuxClToolchain.h>#include <mcuxClCore_Examples.h>#include <mcuxClEls.h>#include <mcuxClExample_ELS_Helper.h>Macros | |
| #define | RSA_KEY_BIT_LENGTH |
| The example uses a 2048-bit key. More... | |
| #define | RSA_KEY_BYTE_LENGTH |
| Converting the key-bitlength to bytelength. More... | |
Functions | |
| static const uint8_t modulus [RSA_KEY_BYTE_LENGTH] | __attribute__ ((aligned(4))) |
| Example value for public RSA modulus N. More... | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClRsa_verify_NoVerify_example) | |
| Performs a session set-up; a call to function mcuxClRsa_verify using mode mcuxClRsa_Mode_Verify_NoVerify; a session clean-up. More... | |
Example of using function mcuxClRsa_verify to perform the RSA signature verification primitive RSAVP1 (public exponentiation and NO padding verification) according to PKCS #1 v2.2.
| #define RSA_KEY_BIT_LENGTH |
The example uses a 2048-bit key.
| #define RSA_KEY_BYTE_LENGTH |
Converting the key-bitlength to bytelength.
|
static |
Example value for public RSA modulus N.
Reference output when calling mcuxClRsa_verify on signature s using the RSA public key pair (N,e) and choosing mode mcuxClRsa_Mode_Verify_NoVerify.
Example value for RSA signature s.
Example value for public RSA exponent e.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClRsa_verify_NoVerify_example | ) |
Performs a session set-up; a call to function mcuxClRsa_verify using mode mcuxClRsa_Mode_Verify_NoVerify; a session clean-up.
| MCUXCLEXAMPLE_OK | The example code completed successfully |
| MCUXCLEXAMPLE_ERROR | The example code failed |
Initialize ELS, Enable the ELS
Destroy Session and cleanup Session
Disable the ELS