Type definitions for the mcuxCsslMemory component. More...
#include <stdint.h>Go to the source code of this file.
Macros | |
| #define | MCUXCSSLMEMORY_STATUS_OK |
| The operation was successful. More... | |
| #define | MCUXCSSLMEMORY_STATUS_EQUAL |
| The two contents of the Memory Compare are equal. More... | |
| #define | MCUXCSSLMEMORY_STATUS_NOT_EQUAL |
| The two contents of the Memory Compare are not equal. More... | |
| #define | MCUXCSSLMEMORY_STATUS_INVALID_PARAMETER |
| A parameter was invalid. More... | |
| #define | MCUXCSSLMEMORY_STATUS_FAULT |
| A fault occurred in the execution. More... | |
| #define | MCUXCSSLMEMORY_KEEP_ORDER |
| Data storing in destination buffer in original order. More... | |
| #define | MCUXCSSLMEMORY_REVERSE_ORDER |
| Data storing in destination buffer with reversed order. More... | |
Typedefs | |
| typedef uint32_t | mcuxCsslMemory_Status_t |
| Type for CSSL Memory status codes. More... | |
Type definitions for the mcuxCsslMemory component.