Parameter structure of elliptic curve of the form, y^2 = x^3 + a*x + b modulo prime p. More...
#include <mcuxClEcc_Types.h>
Data Fields | |
| const uint8_t * | pA |
| [in] pointer to octet string of curve parameter a (< p), of which the length is byteLenP. More... | |
| const uint8_t * | pB |
| [in] pointer to octet string of curve parameter b (< p), of which the length is byteLenP. More... | |
| const uint8_t * | pP |
| [in] pointer to octet string of prime modulus p, of which the length is byteLenP. More... | |
| const uint8_t * | pG |
| [in] pointer to octet string of base point G. More... | |
| const uint8_t * | pN |
| [in] pointer to octet string of base point order n, of which the length is byteLenN. More... | |
| uint32_t | misc |
| [in] packed lengths, via mcuxClEcc_DomainParam_misc_Pack: bits 0~ 7: byteLenP: length of the octet string of curve parameters a, b and p, and x and y coordinates of base point G; bits 8~15: byteLenN: length of the octet string of curve parameter n; bits 16~31: reserved. More... | |
Parameter structure of elliptic curve of the form, y^2 = x^3 + a*x + b modulo prime p.
Each curve parameter is stored as a Big-endian octet string with exact byte length specified. For a small parameter, padding zero(s) is placed in the beginning of the octet string. This structure contains pointers to the octet strings and the lengths.
| const uint8_t* mcuxClEcc_DomainParam_t::pA |
[in] pointer to octet string of curve parameter a (< p), of which the length is byteLenP.
| const uint8_t* mcuxClEcc_DomainParam_t::pB |
[in] pointer to octet string of curve parameter b (< p), of which the length is byteLenP.
| const uint8_t* mcuxClEcc_DomainParam_t::pP |
[in] pointer to octet string of prime modulus p, of which the length is byteLenP.
The leading byte of this octet string shall be nonzero (i.e., != 0x00).
| const uint8_t* mcuxClEcc_DomainParam_t::pG |
[in] pointer to octet string of base point G.
Each coordinate is an octet string of the length byteLenP. The string of x coordinate is followed by the string of y coordinate.
| const uint8_t* mcuxClEcc_DomainParam_t::pN |
[in] pointer to octet string of base point order n, of which the length is byteLenN.
The leading byte of this octet string shall be nonzero (i.e., != 0x00).
| uint32_t mcuxClEcc_DomainParam_t::misc |
[in] packed lengths, via mcuxClEcc_DomainParam_misc_Pack: bits 0~ 7: byteLenP: length of the octet string of curve parameters a, b and p, and x and y coordinates of base point G; bits 8~15: byteLenN: length of the octet string of curve parameter n; bits 16~31: reserved.