Parameter structure for function #mcuxClEcc_PointMult. More...
#include <mcuxClEcc_Types.h>
Data Fields | |
| mcuxClEcc_DomainParam_t | curveParam |
| [in] structure of pointers to curve parameters and length of parameters. More... | |
| const uint8_t * | pScalar |
| [in] pointer to octet string of scalar d, which is of the same format as base point order n. More... | |
| const uint8_t * | pPoint |
| [in] pointer to octet string of EC point Q, which is of the same format as base point G. More... | |
| uint8_t * | pResult |
| [out] pointer to memory area, where the result R = dQ will be exported if PointMult is executed successfully. More... | |
| uint32_t | optLen |
| [in] packed options (reserved): bits 0~31: reserved. More... | |
Parameter structure for function #mcuxClEcc_PointMult.
| mcuxClEcc_DomainParam_t mcuxClEcc_PointMult_Param_t::curveParam |
[in] structure of pointers to curve parameters and length of parameters.
| const uint8_t* mcuxClEcc_PointMult_Param_t::pScalar |
[in] pointer to octet string of scalar d, which is of the same format as base point order n.
| const uint8_t* mcuxClEcc_PointMult_Param_t::pPoint |
[in] pointer to octet string of EC point Q, which is of the same format as base point G.
| uint8_t* mcuxClEcc_PointMult_Param_t::pResult |
[out] pointer to memory area, where the result R = dQ will be exported if PointMult is executed successfully.
It will be stored in the same format as the base point G.
| uint32_t mcuxClEcc_PointMult_Param_t::optLen |
[in] packed options (reserved): bits 0~31: reserved.
CAUTION always set optLen = 0.