Result type of #mcuxClEls_GetHwConfig. More...
#include <mcuxClEls_Common.h>
Data Fields | |
| struct { | |
| uint32_t value | |
| Accesses the bit field as a full word. More... | |
| } | word |
| Access mcuxClEls_InterruptOptionSet_t word-wise. More... | |
| struct { | |
| uint32_t ciphersup:1 | |
| Indicates whether the cipher command is supported. More... | |
| uint32_t authciphersup:1 | |
| Indicates whether the auth_cipher command is supported. More... | |
| uint32_t ecsignsup:1 | |
| Indicates whether the ecsign command is supported. More... | |
| uint32_t ecvfysup:1 | |
| Indicates whether the ecvfy command is supported. More... | |
| uint32_t eckxchsup:1 | |
| Indicates whether the dhkey_xch command is supported. More... | |
| uint32_t keygensup:1 | |
| Indicates whether the keygen command is supported. More... | |
| uint32_t keyinsup:1 | |
| Indicates whether the keyin command is supported. More... | |
| uint32_t keyoutsup:1 | |
| Indicates whether the keyout command is supported. More... | |
| uint32_t kdeletesup:1 | |
| Indicates whether the kdelete command is supported. More... | |
| uint32_t keyprovsup:1 | |
| Indicates whether the keyprov command is supported. More... | |
| uint32_t ckdfsup:1 | |
| Indicates whether the ckdf command is supported. More... | |
| uint32_t hkdfsup:1 | |
| Indicates whether the hkdf command is supported. More... | |
| uint32_t tlsinitsup:1 | |
| Indicates whether the tls_init command is supported. More... | |
| uint32_t hashsup:1 | |
| Indicates whether the hash command is supported. More... | |
| uint32_t hmacsup:1 | |
| Indicates whether the hmac command is supported. More... | |
| uint32_t cmacsup:1 | |
| Indicates whether the cmac command is supported. More... | |
| uint32_t drbgreqsup:1 | |
| Indicates whether the drbg_req command is supported. More... | |
| uint32_t drbgtestsup:1 | |
| Indicates whether the drbg_test command is supported. More... | |
| uint32_t dtrgncfgloadsup:1 | |
| Indicates whether the dtrng_cfg_load command is is supported. More... | |
| uint32_t dtrngevalsup:1 | |
| Indicates whether the dtrng_eval command is supported. More... | |
| uint32_t gdetcfgloadsup:1 | |
| Indicates whether the gdet_cfg_load command is supported. More... | |
| uint32_t gdettrimsup:1 | |
| Indicates whether the gdet_trim command is supported. More... | |
| uint32_t __pad0__:10 | |
| RFU. More... | |
| } | bits |
| Access mcuxClEls_InterruptOptionSet_t bit-wise. More... | |
Result type of #mcuxClEls_GetHwConfig.
Contains ELS configuration values.
| uint32_t mcuxClEls_HwConfig_t::value |
Accesses the bit field as a full word.
| struct { ... } mcuxClEls_HwConfig_t::word |
Access mcuxClEls_InterruptOptionSet_t word-wise.
| uint32_t mcuxClEls_HwConfig_t::ciphersup |
Indicates whether the cipher command is supported.
| uint32_t mcuxClEls_HwConfig_t::authciphersup |
Indicates whether the auth_cipher command is supported.
| uint32_t mcuxClEls_HwConfig_t::ecsignsup |
Indicates whether the ecsign command is supported.
| uint32_t mcuxClEls_HwConfig_t::ecvfysup |
Indicates whether the ecvfy command is supported.
| uint32_t mcuxClEls_HwConfig_t::eckxchsup |
Indicates whether the dhkey_xch command is supported.
| uint32_t mcuxClEls_HwConfig_t::keygensup |
Indicates whether the keygen command is supported.
| uint32_t mcuxClEls_HwConfig_t::keyinsup |
Indicates whether the keyin command is supported.
| uint32_t mcuxClEls_HwConfig_t::keyoutsup |
Indicates whether the keyout command is supported.
| uint32_t mcuxClEls_HwConfig_t::kdeletesup |
Indicates whether the kdelete command is supported.
| uint32_t mcuxClEls_HwConfig_t::keyprovsup |
Indicates whether the keyprov command is supported.
| uint32_t mcuxClEls_HwConfig_t::ckdfsup |
Indicates whether the ckdf command is supported.
| uint32_t mcuxClEls_HwConfig_t::hkdfsup |
Indicates whether the hkdf command is supported.
| uint32_t mcuxClEls_HwConfig_t::tlsinitsup |
Indicates whether the tls_init command is supported.
| uint32_t mcuxClEls_HwConfig_t::hashsup |
Indicates whether the hash command is supported.
| uint32_t mcuxClEls_HwConfig_t::hmacsup |
Indicates whether the hmac command is supported.
| uint32_t mcuxClEls_HwConfig_t::cmacsup |
Indicates whether the cmac command is supported.
| uint32_t mcuxClEls_HwConfig_t::drbgreqsup |
Indicates whether the drbg_req command is supported.
| uint32_t mcuxClEls_HwConfig_t::drbgtestsup |
Indicates whether the drbg_test command is supported.
| uint32_t mcuxClEls_HwConfig_t::dtrgncfgloadsup |
Indicates whether the dtrng_cfg_load command is is supported.
| uint32_t mcuxClEls_HwConfig_t::dtrngevalsup |
Indicates whether the dtrng_eval command is supported.
| uint32_t mcuxClEls_HwConfig_t::gdetcfgloadsup |
Indicates whether the gdet_cfg_load command is supported.
| uint32_t mcuxClEls_HwConfig_t::gdettrimsup |
Indicates whether the gdet_trim command is supported.
| uint32_t mcuxClEls_HwConfig_t::__pad0__ |
RFU.
| struct { ... } mcuxClEls_HwConfig_t::bits |
Access mcuxClEls_InterruptOptionSet_t bit-wise.