Defines the memory consumption for the mcuxClOsccaSm3 component. More...
Go to the source code of this file.
Macros | |
| #define | MCUXCLOSCCASM3_COMPUTE_CPU_WA_BUFFER_SIZE_SM3 |
| Defines the workarea size required for mcuxClOsccaSm3_compute on SM3. More... | |
| #define | MCUXCLOSCCASM3_COMPUTE_CPU_WA_BUFFER_SIZE_MAX |
| Defines the max workarea size required for mcuxClOsccaSm3_compute. More... | |
| #define | MCUXCLOSCCASM3_INIT_CPU_WA_BUFFER_SIZE |
| Defines the max workarea size required for mcuxClOsccaSm3_init. More... | |
| #define | MCUXCLOSCCASM3_PROCESS_CPU_WA_BUFFER_SIZE_SM3 |
| Defines the workarea size required for mcuxClOsccaSm3_process on SM3. More... | |
| #define | MCUXCLOSCCASM3_PROCESS_CPU_WA_BUFFER_SIZE_MAX |
| Defines the max workarea size required for mcuxClOsccaSm3_process. More... | |
| #define | MCUXCLOSCCASM3_FINISH_CPU_WA_BUFFER_SIZE_SM3 |
| Defines the workarea size required for mcuxClOsccaSm3_finish on SM3. More... | |
| #define | MCUXCLOSCCASM3_FINISH_CPU_WA_BUFFER_SIZE_MAX |
| Defines the max workarea size required for mcuxClOsccaSm3_finish. More... | |
| #define | MCUXCLOSCCASM3_MAX_CPU_WA_BUFFER_SIZE |
| Defines the max workarea size required this component. More... | |
| #define | MCUXCLOSCCASM3_CONTEXT_SIZE |
| Defines the context size for streaming hashing interfaces. More... | |
Defines the memory consumption for the mcuxClOsccaSm3 component.