Example for the mcuxClRandomModes component. More...
#include <mcuxClRandom.h>#include <mcuxClRandomModes.h>#include <mcuxClSession.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxClCore_Examples.h>#include <mcuxClEls.h>#include <mcuxClExample_ELS_Helper.h>Functions | |
| static mcuxClRandom_Status_t | RNG_Patch_function (mcuxClSession_Handle_t session, mcuxClRandom_Context_t pCustomCtx, uint8_t *pOut, uint32_t outLength) |
| MCUXCLEXAMPLE_FUNCTION (mcuxClRandomModes_PatchMode_CtrDrbg_AES256_DRG3_example) | |
| Performs an example usage of the mcuxClRandom and mcuxClRandomModes components with patch mode. More... | |
Example for the mcuxClRandomModes component.
|
static |
Destroy Session and cleanup Session
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClRandomModes_PatchMode_CtrDrbg_AES256_DRG3_example | ) |
Performs an example usage of the mcuxClRandom and mcuxClRandomModes components with patch mode.
| true | The example code completed successfully |
| false | The example code failed |
Initialize ELS, Enable the ELS
Destroy Session and cleanup Session
Disable the ELS