Example for the mcuxClRandomModes component. More...
#include <mcuxClRandom.h>#include <mcuxClRandomModes.h>#include <mcuxClSession.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClCore_FunctionIdentifiers.h>#include <mcuxClExample_Session_Helper.h>#include <mcuxClCore_Examples.h>#include <mcuxClEls.h>#include <mcuxClExample_ELS_Helper.h>Macros | |
| #define | CEILING(x, y) |
| #define | OUT_BUFFER_SIZE |
Functions | |
| MCUXCLEXAMPLE_FUNCTION (mcuxClRandomModes_TestMode_CtrDrbg_AES256_PTG3_example) | |
| Performs an example usage of the mcuxClRandom and mcuxClRandomModes components with test mode. More... | |
Example for the mcuxClRandomModes component.
| MCUXCLEXAMPLE_FUNCTION | ( | mcuxClRandomModes_TestMode_CtrDrbg_AES256_PTG3_example | ) |
Performs an example usage of the mcuxClRandom and mcuxClRandomModes components with test mode.
| true | The example code completed successfully |
| false | The example code failed |
Initialize ELS, Enable the ELS
Destroy Session and cleanup Session
Disable the ELS