![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
This file implement audio source element of pcmrtos. More...
Functions | |
| AudioSrcStreamErrorType | audiosrc_pcmrtos_init_params (ElementAudioSrc *audio_src_element) |
| This function initializes the PCM manager device parameters. More... | |
| AudioSrcStreamErrorType | audio_src_pcmrtos_init_device (ElementAudioSrc *audio_src_element) |
| Audio source pcmrtos device initialization function. More... | |
| AudioSrcStreamErrorType | audio_src_pcmrtos_deinit_device (ElementAudioSrc *audio_src_element) |
| Audio source pcmrtos device deinitialization function. More... | |
| AudioSrcStreamErrorType | audio_src_pcmrtos_start_device (ElementAudioSrc *audio_src_element) |
| Audio source pcmrtos device start device function. More... | |
| AudioSrcStreamErrorType | audio_src_pcmrtos_stop_device (ElementAudioSrc *audio_src_element) |
| Audio source pcmrtos device stop device function. More... | |
| AudioSrcStreamErrorType | audio_src_pcmrtos_read_device (ElementAudioSrc *audio_src_element, uint32_t length, StreamBuffer *buf) |
| Audio source pcmrtos device read function. More... | |
| AudioSrcStreamErrorType audiosrc_pcmrtos_init_params | ( | ElementAudioSrc * | audio_src_element | ) |
| audio_src_element | pointer to an audio src instance |
| AUDIO_SRC_SUCCESS | successful |
| AUDIO_SRC_ERROR_INVALID_ARGS | invalid argument |
| AUDIO_SRC_FAILED | failed to get pcm manager file handle |
| AudioSrcStreamErrorType audio_src_pcmrtos_init_device | ( | ElementAudioSrc * | audio_src_element | ) |
| audio_src_element | Audio source pointer |
| AudioSrcStreamErrorType audio_src_pcmrtos_deinit_device | ( | ElementAudioSrc * | audio_src_element | ) |
| audio_src_element | Audio source pointer |
| AudioSrcStreamErrorType audio_src_pcmrtos_start_device | ( | ElementAudioSrc * | audio_src_element | ) |
| audio_src_element | Audio source pointer |
| AudioSrcStreamErrorType audio_src_pcmrtos_stop_device | ( | ElementAudioSrc * | audio_src_element | ) |
| audio_src_element | Audio source pointer |
| AudioSrcStreamErrorType audio_src_pcmrtos_read_device | ( | ElementAudioSrc * | audio_src_element, |
| uint32_t | length, | ||
| StreamBuffer * | buf | ||
| ) |
| audio_src_element | Audio source pointer |
| length | Length to be read |
| buf | buffer pointer |