![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
Files | |
| file | audio_sink_pcmrtos.c |
| This file contains the implementation for the pcmrtos Audio Sink Interface. | |
| file | audio_sink_pcmrtos.h |
| This file contains the definitions for the PCM manager Audio Sink Interface. | |
| file | audio_src_pcmrtos.c |
| This file implement audio source element of pcmrtos. | |
| file | audio_src_pcmrtos.h |
| This is the header file for the audio source element of pcmrtos. | |