![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
Files | |
| file | streamer_audiosrc.c |
| Implementation of streamer audio source support. | |
| file | streamer_audiosrc.h |
| This file contains the definition of the streamer audio source functionality. | |
| file | streamer_fs.c |
| Implementation of streamer file system support. | |
| file | streamer_fs.h |
| This file contains the definition of the streamer filesystem functionality. | |
| file | streamer_mic2file.h |
| This file contains the definition of the streamer audio source functionality. | |
| file | streamer_opusmem2mem.c |
| Implementation of tempoprary Opus memory-to-memory pipeline. | |
| file | streamer_opusmem2mem.h |
| This file contains headers for the temporary memory-to-memory pipeline with Opus encoder. | |