![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
Files | |
| file | pad.c |
| This file contains the streamer element pad implementation. | |
| file | pad.h |
| This file contains the definition of an element pad object. | |
| file | pipeline.c |
| The implementation for the Af Streamer pipeline. | |
| file | pipeline.h |
| This file contains the definition of the pipeline object. | |
| file | streamer.c |
| Af Streamer implementation. | |
| file | streamer.h |
| Contains common types and functions used throughout the streamer. | |
| file | streamer_element.c |
| Implementation of streamer element. | |
| file | streamer_element.h |
| Header for Streamer Element. | |
| file | streamer_msg.c |
| Implementation of streamer message handlers. | |