![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
Files | |
| file | error.h |
| Contains common error codes and definitions. | |
| file | file_utils.h |
| This file provides file manipulation functions. | |
| file | general_utils.h |
| This file provides general helper functions. | |
| file | maestro_logging.h |
| Contains maestro_logging prototypes and definitions for the connected radio. | |
| file | ringbuffer.h |
| Implements a data ringbuffer. | |
| file | streamer_api.h |
| Streamer API header. Public APIs for using the maestro streamer framework. | |
| file | streamer_element_properties.h |
| Header for streamer element properties. | |
| file | streamer_message.h |
| file | streamer_pcm.h |
| Streamer PCM API header. Public APIs for configuring the input/output PCM interfaces. | |