This file includes defines, enums and typedefs for file sink.
More...
|
|
#define | DEFAULT_FILESINK_LOCATION "rec.pcm" |
| | Default file sink location (file name)
|
| |
◆ FILE_Dump_Task()
| void FILE_Dump_Task |
( |
void * |
param | ) |
|
◆ filesink_init_element()
| int32_t filesink_init_element |
( |
StreamElement * |
element | ) |
|
- Parameters
-
| element | an element which is created by parent element |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
◆ filesink_set_location()
| int32_t filesink_set_location |
( |
ElementHandle |
element, |
|
|
char * |
path |
|
) |
| |
- Parameters
-
| element | element handle |
| path | pointer to a file path |
- Returns
- StreamReturnType
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |
◆ filesink_set_write_mode()
| int32_t filesink_set_write_mode |
( |
ElementHandle |
element, |
|
|
uint8_t |
write_mode |
|
) |
| |
- Parameters
-
| element | element handle |
| write_mode | write mode raw (or) packet header |
- Returns
- : StreamReturnType
- Return values
-
| STREAM_OK | if successful |
| STREAM_ERR_INVALID_ARGS | means invalid arguments |