![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
Maestro audio framework provides instruments for playback and capture of different audio streams. In order to do that the framework uses API for creating various audio and voice pipelines with the support of media and track information. This document describes the framework in its detail, and the usage of API for pipeline creation using different elements. The framework needs an operating system in order to create different tasks for audio processing and communication with the application.
A high-level block diagram of the streamer used in Maestro is shown below. An element is the most important class of objects in the streamer (see streamer_element.c). A chain of elements will be created and linked together when a pipeline is created. Data flows through this chain of elements in form of data buffers. An element has one specific function, which can be the reading of data from a file, decoding of this data, or outputting this data to a sink device. By chaining together several such elements, a pipeline is created that can do a specific task, for example, the playback.
The pipeline itself is created within the streamer_create API using the streamer_create_pipeline call. In the underlying streamer_msg_create_pipeline call the correct pipeline type is selected and then the specific streamer_build_pipeline is used. In order to create a new user defined pipeline it is necessary to create a new source file in the pipeline folder. The new pipeline type needs to be added into the StreamPipelineType enum in the streamer_api.h file. Then in the streamer_msg_create_pipeline function it is necessary to add a case for that particular pipeline in the switch(streamer_msg->pipeline_type) statement. The streamer_build_new_pipeline function needs to implement the building of the desired pipeline using following API:
create_pipeline - allocate memory for a new pipeline and initialize the maximum elementscreate_element - create an element with the desired type, initialize its source and sink padsadd_element_pipeline - add the created elements into the pipelinelink_elements - connect the elements together linking the source pads to sink pads and the other way roundThen it is also necessary to implement a new function for destroying the pipeline and register it in the streamer_msg_destroy_pipeline function, i.e. stream_destroy_new_pipeline using following API:
unlink_elements - disconnect the elementsremove_element_pipeline - remove the elements from the pipelinedestroy_element - destroy the elements and free the memorydestroy_pipeline - destroy the pipeline and free the memoryPads are elements' inputs and outputs. A pad can be viewed as a "plug" or "port" on an element where links may be made with other elements, and through which data can flow to or from those elements. Data flows out of an element through a source pad, and elements accept incoming data through a sink pad. Source and sink elements have only source and sink pads, respectively. For detailed information about pads, please see the API reference from pad.c.
The streamer (the core of the framework) provides several mechanisms for communication and data exchange between the application, a pipeline, and pipeline elements:
Maestro framework uses a common codec interface for decoding purposes and a common encoder interface for encoding. Those interfaces encapsulate the usage of specific codecs.
The Common Codec Interface is the intended interface for all used decoders. The framework will integrate a CCI decoder element into the streamer to interface with all decoders.
cci_extract_meta_data must be called before any other Codec Interface APIs. This API extracts the metadata information of the codec and fills this information in the file_meta_data_t structure. The file_meta_data_t structure must be allocated by the application.codec_get_mem_info gets the memory requirement based on the specific decoder stream type. It returns the size in bytes of the specific codec. The user of the decoders must allocate memory of this size and this memory is used by the initialization API. The user or application must pass this allocated memory pointer to the init API.codec_init must be called before the codec’s decode API. This API calls the codec-specific initialization function based on the codec stream type. This API allocates the memory to the codec main structure and also initializes the codec main structure parameters. It also registers the call back functions to the codec which will be used by the codec to read or seek the input stream.codec_decode is the main decoding API of the codec. This API calls the codec-specific decoding function based on the codec stream type. This API decodes the input raw stream and fills the PCM output samples into codec output PCM buffer. This API gives the information about the number of samples produced by the codec and also gives the pointer of the codec output PCM samples buffer.codec_get_pcm_samples must be called after the codec’s decode API. This API calls the codec specific Get PCM Sample API based on the codec stream type. This API gets the PCM samples from the codec in constant block size and fills them into the output PCM buffer. It returns the number of samples get from the codec and also gives the pointer of the output PCM buffer.codec_reset calls the codec specific reset API base on stream type and resets the codec.codec_seek accepts the seek bytes offset converted from the time by application. This API calls the decoder’s internal seek API to calculate the actual seek offset which frame boundary aligns. This API returns the actual seek offset.The basic sequence to use a decoder with the CCI is shown below:

This section explains how to integrate a new decoder in the Common Codec Interface. The CCI assumes the decoder library to be used is in the libs folder of the maestro framework. The CCI is just a wrapper around a specific implementation. The decoder is expected to be extended as needed to meet the APIs described above.
libs folder.VORBIS_CODEC macro in audio_cfg.h file.libs folder.ccidec_extract_meta_data API (in codecextractmetadata.c file) to call VORBIS Decoder extract metadata API.Please see the following section about the cei.
The memory usage of the framework (data obtained from IAR compiler) in bytes is:
| Section | Size |
|---|---|
| .text | 77678 |
| .bss | 5013 |
The performance of the decoder was measured using the real hardware platform (RT1060).
| Pipeline type | Performance MIPS of codec (in MHz) |
|---|---|
| audio source -> audio sink | ~10.26 MHz |
| audio source -> file sink | ~9.84 MHz |
| file source (8-channel PCM) -> audio sink | ~16.5 MHz |
For performance details about the supported codecs please see MP3 decoder and WAV decoder documents.
For opus decoder documentation please see following link: opus.
The following library is used for gaining information from the Ogg Opus audio streams: opusfile.