|
| static int32_t | netbufsrc_change_state (StreamElement *element, PipelineState state) |
| | Function handles the state change of the element in a pipeline. More...
|
| |
| static uint8_t | netbufsrc_handle_src_event (StreamPad *pad, StreamEvent *event) |
| | Function handles the events of the element source pad. More...
|
| |
| static uint8_t | netbufsrc_handle_src_query (StreamPad *pad, StreamQuery *query) |
| | Function Description: This function is the empty impl of the src pad query handler. More...
|
| |
| static uint8_t | netbufsrc_src_activate_pull (StreamPad *pad, uint8_t active) |
| | Function activates or deactivates the netbufsrc source pad in PULL mode. More...
|
| |
| static uint8_t | netbufsrc_src_activation_handler (StreamPad *pad, uint8_t active) |
| | queue src pad activatation handler. Activation is handled by the peer sink pad, this should just handle the deactivation. More...
|
| |
| static FlowReturn | netbufsrc_pull (StreamPad *pad, StreamBuffer *buffer, uint32_t size, uint32_t offset) |
| | Function is the pull function of the netbufsrc source pad in SCHEDULING_PULL mode. It reads the size of data from the offset to buffer. More...
|
| |
| static int32_t | netbufsrc_get_property (StreamElement *element_ptr, uint16_t prop, uint32_t *val_ptr) |
| | This function get memory source element properties. More...
|
| |
| static int32_t | netbufsrc_set_property (StreamElement *element_ptr, uint16_t prop, uintptr_t val) |
| | This function set memory source element properties. More...
|
| |
| int32_t | netbufsrc_init (StreamElement *element) |
| | this function initializes the netbuf source element and source pad. all the pad's handlers are intialized. More...
|
| |
| static FlowReturn | netbufsrc_read (ElementNetbufSrc *netbufsrc, int32_t offset, int32_t length, StreamBuffer *buf) |
| | Reads the data from the memory array specified by the element. NOTE: Function may or may not be able to read the required length of data. More...
|
| |