![]() |
Maestro Audio Framework v 1.5
NXP Semiconductors
|
PCM Source device information.
#include <audio_src_pcmrtos.h>
Data Fields | |
| pcm_rtos_t * | pcm_handle |
| Pointer to pcm handle. | |
| char * | unaligned_buf [AUDIO_SRC_BUFFER_NUM] |
| Pointers to unaligned buffers. | |
| char * | audbuf [AUDIO_SRC_BUFFER_NUM] |
| Pointers to aligned audio buffers. | |
| uint32_t | buff_size [AUDIO_SRC_BUFFER_NUM] |
| Size of the data in the audbuf. | |
| uint8_t | buff_index |
| Current buffer index. | |
| uint8_t | device_state |
| Device state. | |
| bool | init_params_done |
| Initialization done flag. | |
| bool | continuous_read |
| Continuous read flag. | |